hello support team
we have a problem about clk synthesizer.
when we tested ad9864 in my test room, every thing is ok and don't move the ad9864 clk synth.
but when we go to field test (like as free space and In the vicinity of the sun) after a short time, the clock synthesizer start moving. after shutting own and cooling the system, start it again and in first time the clk synthesizer is ok. whit increase the temperature and system running, start moving again.
all test repeat with ad9864 eval board and same result achieved.
could you help me about that problem???
regards
Hello,
Assuming the FREF frequency remains stable over temp than the likely cause is that the PLL is falling out of lock at higher temp. Referring to figure 41 of the datasheet, the DC voltage across the…
Assuming the FREF frequency remains stable over temp than the likely cause is that the PLL is falling out of lock at higher temp. Referring to figure 41 of the datasheet, the DC voltage across the varactor should remain a few 100 mV above AGND and below VDDC. At room temperature, the design goal is to have the DC voltage centered around mid-supply to accommodate temperature drift while staying in its linear region. Note that if the DC voltage is high, the PLL loop is trying to decrease the varactor contribution capacitance which reduced the value of the series Cv,Cosc contribution thus one could try reducing the Cosc by a few pF. Conversely........it DC voltage is low, the PLL loop is trying to increase the varactor contribution so one could try increasing the Cosc by a few pF.
If PLL stability over temperature is the issue than one can increase the KVCO of the oscillator such that a lower dc voltage change would be required to support the temperature drift hence preventing the DC voltage across the varactor from railing near AGND or VDDC. For an RLC tank circuit with the inductor and varactor contributing to the series R...........the Q=1/R*sqrt(L/C) thus decreasing L and increasing C proportionally should decrease the Q while maintain same resonance frequency.
https://toshiba.semicon-storage.com/us/product/diode/rf-diode/detail.1SV228.html