Post Go back to editing

AD9231, AD9573

Thread Summary

The user inquires about using the AD9573 as a low-power clock source for the AD9231, specifically for the 100MHz output. The final answer confirms that the AD9573 can be used, with all VDD pins (including VDD33) set to 3.3V ±10% and GND33 connected to ground. The 33M pin can be left floating if the 33MHz output is not used. The AD9231's clock divider can handle the 100MHz input by dividing it by an integer value between 1 and 8.
AI Generated Content

Hello,

I'm looking for a clock wich I can use for the AD9231. It needs to be a low power device for my design. Is the AD9573 suitable for that? I'll only need the 100MHz output of the AD9573. To wich level do I have to connect the VDD33, 33M and GND33 pins if I won't use the 33MHz output?