Post Go back to editing

AD9680:Spurs around sub-harmonics of the sample clock

FormerMember
FormerMember

I am using AD9680 and HMC7044 toghether.

We are seeing  spur in the FFT of the ADC output. It appears that the spur is around fs/2.  if the fundamental signal into the ADC is at 200 MHz and 1000 MHz is the sampling clock. I am seeing a spur at 300MHz. This appears to come from ( fs/2-Fin).

1)Can you explain how to reduce this spur?

2)which type of clock is better for 1000MHz sampling clock (LVDS or LVPECL) and explain config clock

Thanks,

Top Replies

Parents Reply Children
No Data