Post Go back to editing

AD9680:Spurs around sub-harmonics of the sample clock

Anonymous
Anonymous

    I am using AD9680 and HMC7044 toghether.

    We are seeing  spur in the FFT of the ADC output. It appears that the spur is around fs/2.  if the fundamental signal into the ADC is at 200 MHz and 1000 MHz is the sampling clock. I am seeing a spur at 300MHz. This appears to come from ( fs/2-Fin).

    1)Can you explain how to reduce this spur?

    2)which type of clock is better for 1000MHz sampling clock (LVDS or LVPECL) and explain config clock

    Thanks,

    Top Replies