Post Go back to editing

LTM9013 datasheet clarification request

Hi,

I'm considering designing a board using the LTM9013 and require some help.

In the datasheet on page 4, the REF input (demodulator adjust input) specifies a min and max  range of 0.4 - 0.7 volts. On the other hand the reference schematic on page 31 connects to a voltage that I think is half of VDD (1.8V) which is 0.9V.

What is the correct input range for this pin?

Thanks.

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.