AD9287 Dataout frequency not right

I  have gotten a problem with AD9287ABCPZ-100, as follows,

According to the Timing diagram of AD9287 ,when my input  clock is 20Mhz, the frequency of dataout should be 80Mhz ,and the bit clock(DCO) should be 80Mhz ,frame clock(FCO) should be 20Mhz .

But in fact ,the frequency of DCO and DCO is right ,but the frequence of dataout is 20Mhz,too. So it makes me confused ,Idont know which question leads to this. SO I need a help.

Thanks for your answer !

Parents Reply
  • 0
    •  Analog Employees 
    on Mar 25, 2019 3:53 PM over 1 year ago in reply to XIAWEN

    Hi Xiawen,

    Thank you for using the AD9287.

    I agree with what you state from the AD9287 datasheet timing diagram.

    Would you please double-check the signals you are probing? I believe it is impossible for FCO frequency to be greater than DCO frequency, and FCO frequency to be the same as the serial data output waveform frequency.

    Thank you.

    Doug

Children
  • Thanks for your patient reply. In fact ,I check the data signals, then I find that when my analog input is equal to 0, the frequency of data_out is equal to FCO, while even if it is not 0, the frequency of data_ out  is  higher ,but I  can't tell it's eight times the frequency of the FCO. Here is the diagram that analog input is not equal to zero when FCO = 20Mhz.Thank you!

  • Dear Doug,

    What I said is that my FCO and DCO is right,the FCO diagram I showed is 50ns/div, eqaul to 10 times of DCO.

  • 0
    •  Analog Employees 
    on Mar 27, 2019 3:00 PM over 1 year ago in reply to XIAWEN

    Hi Xiawen,

    Sorry, it seems that I misunderstood your question. OK, FCO and DCO frequencies are correct.

    Do you have SPI control of your AD9287? If so can you try one of the stored digital test patterns to look at your output data? Sometimes noise can cause one or more of the lower order bits to flip randomly which can make observation of the output frequency more difficult.

    For example, to output a checkerboard pattern you would do the following SPI sequence:

    Write Register 0x0D = 0x04 #select checkerboard test pattern
    Write Register 0xFF = 0x01 #transfer bit to put previous SPI writes into effect

    Is this something you can try?

    Thanks,

    Doug

  • Sorry,Doug.

    This is my first time to design a PCB, so I didn't add SPI  communication between FPGA and AD9287.So I can't finish this.. Is there any another way?

  • 0
    •  Analog Employees 
    on Mar 28, 2019 5:07 PM over 1 year ago in reply to XIAWEN

    Hi Xiawen,

    Yes, there is another way. If you designed your board for no SPI communication, CSB is tied high, correct?. In that case do you have the ability to tie the SCLK/DTP (pin 28) high or low? When CSB is tied high at ADC power-up, then the SCLK/DTP pin functions as a control bit for outputting a known test pattern.

    SCLK/DTP pin low: Normal ADC operation
    SCLK/DTP pin high (AVDD): shift out 1000 0000 on each channel
    Please see the AD9287 datasheet Table 12 for more information.

    Do you have the ability to control the voltage on SCLK/DTP?

    Thank you.

    Doug