HMCAD1511 BOM

Hi, I was wondering if i could receive a BOM for the evaluation module of the HMCAD1511? I also wanted to ask if we could solder the missing PLL, capacitors, and resistors to generate a 1GHz clock and if so, which resistors and capacitors need to be soldered and which can be omitted? In the datasheet on page 11 it looks as if we are able to do this but I just want to confirm. I am attaching the datasheet to this message. Thank you! www.analog.com/.../hardware-users-guide-140-00036-00-15xx.pdf



Added a sentence asking about which resistors and capacitors we need to connect
[edited by: rmeruvia at 8:17 PM (GMT 0) on 10 Feb 2019]
  • 0
    •  Analog Employees 
    on Feb 20, 2019 10:31 PM

    Hi,

    The components identified as "Do Not Populate" (such as the onboard Clk PLL-U2) in the List of Materials on page 8 of the Hardware-Users-Guide you linked above were never productized or supported by the original HMCAD1511/HMCAD1520 Development Team. Unfortunately we have no further details on these uninstalled/unsupported components.

    Best Regards,

    TonyM