AD9653

Hi! 

We are interested in the AD9653 converter. We understand that we need the pack AD9653 plus HSC-ADC-EVALCZ to evaluate the ADC, is that right? If so, how much it costs? and more important, it is included some VHDL code exmaple to control the AD9653?

Thanks in advance,

Juan.

 

Parents
  • 0
    •  Analog Employees 
    on Nov 20, 2018 4:22 AM in reply to Juanelete

    Hi Juan,

    Here is a discussion about using the FMC interposer with the AD9633, which is the 12bit version of the AD9653 https://ez.analog.com/fpga/f/q-a/84486/interfacing-ad9633-eval-board-with-ml605-using-an-adi-working-reference-design/84700#84700 . The AD9653 and AD9633 use the same evaluation board.

    Regarding the sample FPGA code, the AD9681 is a 14bit 8-channel ADC that uses the same LVDS outputs as the AD9653. The FPGA capture board we use for the AD9681 is the HSC-ADC-EVALDZ and HSC-ADC-EVALEZ. Here is an example of AD9681 capture FPGA code written for Virtex6.

    https://ez.analog.com/data_converters/high-speed_adcs/f/q-a/21250/eval-ad9681-hsc-adc-evaldz

    Of course the pin assignments are specific to AD9681, but the capture method also would apply to the AD9653. This code is provided freely, as-is, and without guarantee.

    Thanks,

    Doug

  • Thanks Dougl and don't worry,

    So, I understand that we could evaluate the AD9653-125EBZ board using an own virtex6 based board, as long as it has a FMC port, using the FMC interposer (EVAL-ADC-FMC-INT), isn't it? 

    Another option would be to use the HSC-ADC-EVALDZ (which has a virtex6) with the AD9653-125EBZ and modify the pin assignment, isn't it?

    If so, where can we purchase one of these FMC interposer and theHSC-ADC-EVALDZ? Because I can not find the option to buy it in the product pages and in many distributors they seams to be not available.

    Thanks

    Juan.

  • 0
    •  Analog Employees 
    on Nov 26, 2018 5:42 PM in reply to Juanelete

    Hi Juan,

    Using the EVAL-ADC-FMC-INT with AD9653-125EBZ and your own FPGA board, would require some additional steps.

    • As mentioned before, you would need to do some manual modifications (soldering) to the EVAL-ADC-FMC-INT.
    • You would still need to write your own FPGA program for the FPGA board you choose. Even if the board uses Virtex6, you would still need to write your own program. Of course you could use our code as an example to start from.
    • You would need to check that the EVAL-ADC-FMC-INT mechanically fits with the FPGA board you choose. The FMC connector will fit, but I do not know about any other mechanical incompatibilities that might be there.
    • Also, the EVAL-ADC-FMC-INT is discontinued and is no longer in production.

    Using the AD9653-125EBZ with HSC-ADC-EVALDZ has another set of challenges.

    • The HSC-ADC-EVALDZ is no longer in production, so it would be difficult to find one.
    • Even if you had a HSC-ADC-EVALDZ, you would need to write your own FPGA program. As you noted, the pin assignments are different and the AD9681. I'm not sure what else you would need to change.

    As noted both the HSC-ADC-EVALDZ and EVAL-ADC-FMC-INT are no longer in production. For the EVAL-ADC-FMC-INT, I know this is not an attractive option but the information to build your own board (layout, schematic, BOM) is on the website.

    I'm sorry but I think the easiest would be for you to buy an HSC-ADC-EVALCZ..

    Doug

Reply
  • 0
    •  Analog Employees 
    on Nov 26, 2018 5:42 PM in reply to Juanelete

    Hi Juan,

    Using the EVAL-ADC-FMC-INT with AD9653-125EBZ and your own FPGA board, would require some additional steps.

    • As mentioned before, you would need to do some manual modifications (soldering) to the EVAL-ADC-FMC-INT.
    • You would still need to write your own FPGA program for the FPGA board you choose. Even if the board uses Virtex6, you would still need to write your own program. Of course you could use our code as an example to start from.
    • You would need to check that the EVAL-ADC-FMC-INT mechanically fits with the FPGA board you choose. The FMC connector will fit, but I do not know about any other mechanical incompatibilities that might be there.
    • Also, the EVAL-ADC-FMC-INT is discontinued and is no longer in production.

    Using the AD9653-125EBZ with HSC-ADC-EVALDZ has another set of challenges.

    • The HSC-ADC-EVALDZ is no longer in production, so it would be difficult to find one.
    • Even if you had a HSC-ADC-EVALDZ, you would need to write your own FPGA program. As you noted, the pin assignments are different and the AD9681. I'm not sure what else you would need to change.

    As noted both the HSC-ADC-EVALDZ and EVAL-ADC-FMC-INT are no longer in production. For the EVAL-ADC-FMC-INT, I know this is not an attractive option but the information to build your own board (layout, schematic, BOM) is on the website.

    I'm sorry but I think the easiest would be for you to buy an HSC-ADC-EVALCZ..

    Doug

Children
No Data