Eval01-HMCAD1511 Bill Of Materials

Hi everybody,

i am a little bit in trouble with the HMCAD1511 evaluation board. I am using this board connected to my Zedboard and i want to generate the 1GHz sampling clock on board.

Since the Zedboard i have is not capable of creating such signal, i  want to solder the PLL chip on the HMCAD1511 board. I searched on the Hardware User Guide of the board

(here is the link to the document: https://www.analog.com/media/en/technical-documentation/evaluation-documentation/hardware-users-guide-140-00036-00-15xx.pdf)

and in the part list is only referred as "do not mount" component.

Does anyone have the complete part list for the board? it will really save me time.

Thanks for the help.

Parents Reply
  • Hi Ihjhit !

    I am a little bit confused by the question but i'll try to answer.

    When you want to sample at 1 Gbps with this chip, you have to feed it with an external 1 GHz clock. That said, if you are using the single channel mode at 1G the chip uses all 4 internal ADC interleaved (so each of them is sampling at 250 MHz  with a known phase shift wrt to the others). So in the fastest mode that the chip can handle the max sample frequency that the single ADC handle is 250M but the whole throughput will be 250M x 4.

    Hope this solve your doubt.

Children
No Data