Post Go back to editing

AD9684 decimation ratio

Hi,

I need to set decimation ratio to decimated by one but I can only set to 2, 4, 8 (I don't need 16).

I have setup AD9684 registers as below to capture real signal only on 2 channels.

chip application mode (register 0x200) = 0x22

chip decimation ratio (register 0x201) = 0x00

DDC0 control (register 0x310) = 0x5B

DDC0 input selection(register 0x311) = 0x00

DDC1 control (register 0x330) = 0x5B

DDC1 input selection(register 0x331) = 0x05

output mode control(register 0x559) = 0x01 (tied to OVR bit)

Output Mode (register 0x561) = 0x00

LVDS Output Mode (register 0x568) = 0x01

all other registers are set as default.

is there any specific setting I need to do?

Parents Reply Children
  • I am using ILA ip core in VIVAdo to check the input and output data of axi-ad9684.

    when I probe dc_rawdata_0_s & adc_rawdata_1_s at the output of SERDES module, data is the same every two clocks.

    also, when I capture data with the pc, every 32 bits is repeated.