Post Go back to editing

AD9655 Anlog input interface through Transformers

HI,

   I Have some queries regarding AD9655 Evaluation schematics ,Please clarify the below queries.

   1. Evaluation schematic inputs connected only Ain+ why?

   2. If i am getting signal from  Board. using Differential driver i have to use AIN+ and AIN-or i have to convert to Single ended again in my board

   3. Please provide schematics for Differential input with transformer coupling. 

Parents
  • 1. that is the schematic we used to test the AD9655 in the lab. our signal generators are single ended and we need a way to convert them to differential. 

    2. you can remove the transformers and place an additional SMA connector to enable differential connection

    3. the same schematic can be used to convert to a fully differential front end.

  • i am planning to connect on my boar like below Please suggest if i am wrong

    VIN+ Connected to Transformer through 0.1uF

    VIN- Connected to other end of Transformer through 0.1uF in the place of AGND

    Below attached Schematic Please suggest if i am wrong

Reply
  • i am planning to connect on my boar like below Please suggest if i am wrong

    VIN+ Connected to Transformer through 0.1uF

    VIN- Connected to other end of Transformer through 0.1uF in the place of AGND

    Below attached Schematic Please suggest if i am wrong

Children
No Data