Post Go back to editing

AD9208: Harmonic of Decimated FS mixes with NCO

Hi,

I am using AD9208 for one of my application. I am using AD9208-3000EBZ+ADS7-V2EBZ for the evaluation

In my setup Fs is 3GHz

Decimation Rate is 8

Decimated Fout (Decimated Fs) is 375MHz (3GHz/8)

NCO is 702MHz

RF In to the ADC is 800MHz

I have observed that there is spur in the output spectrum that is arising from mixing of the harmonic of Fout with NCO.

For the above setup there is spur at 48MHz.

2*375MHz - 702MHz = 48MHz

The snapshot of the ACE setup and the output spectrum is attached.

Is this spur expected? What can be done to minimize this spur?

Regards,

Dwijen

Parents
  • Hi Umesh,

    Thanks a lot for the explanation.

    I have observed that,

    In the snap shot you sent from your lab on Dec 22 has this spur present. However the amplitude you observe is lower than what we are observing. I have reattached the snapshot in below.

    The amplitude of the 48MHz spur in the below snapshot is -98dBFS. The amplitude we are observing is around -94dBFS.

    I have also observed that this spur amplitude is changing almost dB by dB with clock amplitude.

    I have set clock power to be 10dBm on the MXG sig gen.

    What clock power was used for the below snapshot in your lab?

    Also is there a spec on the clock phase noise for AD9208?

    Regards,

    Dwijen

Reply
  • Hi Umesh,

    Thanks a lot for the explanation.

    I have observed that,

    In the snap shot you sent from your lab on Dec 22 has this spur present. However the amplitude you observe is lower than what we are observing. I have reattached the snapshot in below.

    The amplitude of the 48MHz spur in the below snapshot is -98dBFS. The amplitude we are observing is around -94dBFS.

    I have also observed that this spur amplitude is changing almost dB by dB with clock amplitude.

    I have set clock power to be 10dBm on the MXG sig gen.

    What clock power was used for the below snapshot in your lab?

    Also is there a spec on the clock phase noise for AD9208?

    Regards,

    Dwijen

Children
No Data