Post Go back to editing

AD9208: Harmonic of Decimated FS mixes with NCO

Hi,

I am using AD9208 for one of my application. I am using AD9208-3000EBZ+ADS7-V2EBZ for the evaluation

In my setup Fs is 3GHz

Decimation Rate is 8

Decimated Fout (Decimated Fs) is 375MHz (3GHz/8)

NCO is 702MHz

RF In to the ADC is 800MHz

I have observed that there is spur in the output spectrum that is arising from mixing of the harmonic of Fout with NCO.

For the above setup there is spur at 48MHz.

2*375MHz - 702MHz = 48MHz

The snapshot of the ACE setup and the output spectrum is attached.

Is this spur expected? What can be done to minimize this spur?

Regards,

Dwijen

Parents
  • Hi Dwijen,

    Thanks for the explanation. We here do not see this spur.

    I am concerned that you are seeing this spur even when RF is turned off. What you see at 48MHz/3GSPS and 45.75MHz/2.991GSPS is the DC spur that has been rotated, and filtered. I have seen that in some cases this could be a possibility. To prove this, what we could do is to get the DDC setting to decimate by 16. And try the same thing (DDC spectrum without the RF).

    FYI, we set the AD9208 in our lab and didnt see the spur that high. See below the full bandwidth and DDC spectrums.

    Full Bandwidth

    DDC

    From our spectrum I have to believe this spur at 48MHz is either a harmonic or the DC spur. The ACE program correctly identifies the H3 Image as falling on -100MHz at 65dBc. This power matches the H3 power in the FBW mode plot.

    We will continue to do more testing. However, we are going to be shutdown for the week and wont be back until after the New Year's.

    Thanks

    Umesh

Reply
  • Hi Dwijen,

    Thanks for the explanation. We here do not see this spur.

    I am concerned that you are seeing this spur even when RF is turned off. What you see at 48MHz/3GSPS and 45.75MHz/2.991GSPS is the DC spur that has been rotated, and filtered. I have seen that in some cases this could be a possibility. To prove this, what we could do is to get the DDC setting to decimate by 16. And try the same thing (DDC spectrum without the RF).

    FYI, we set the AD9208 in our lab and didnt see the spur that high. See below the full bandwidth and DDC spectrums.

    Full Bandwidth

    DDC

    From our spectrum I have to believe this spur at 48MHz is either a harmonic or the DC spur. The ACE program correctly identifies the H3 Image as falling on -100MHz at 65dBc. This power matches the H3 power in the FBW mode plot.

    We will continue to do more testing. However, we are going to be shutdown for the week and wont be back until after the New Year's.

    Thanks

    Umesh

Children
No Data