• LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents Why would I choose to use DDS for synthesizing a signal rather than a PLL?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • -DDS: FAQ
    • Are any of your DDS products space qualified?
    • Are there any specific recommendations regarding via fill material in the circuit board for the thermally enhanced package styles associated with some ADI DDSs?
    • Can I use a DDS to produce modulation waveforms?
    • DDS Features Chart
    • DDS Tutorial - Introduction to DDS
    • DDS Tutorial - SINC Envelope Correction
    • DDS Tutorial - The Accumulator
    • DDS Tutorial - The Angle-to-Amplitude Converter
    • DDS Tutorial - The DAC
    • DDS Tutorial - The DAC Reconstruction Filter
    • DDS Tutorial - The DDS in Action
    • DDS Tutorial - User Guide
    • DIRECT DIGITAL SYNTHESIS (DDS) SUPPORT COMMUNITY
    • Do you recommend a linear or switching power supply?
    • Does your DDS evaluation software work on Windows XP/Vista/7/8 32-bit/64-bit?
    • How do ADI's DDS engines compare to FPGA-based DDS engines?
    • How does the REF CLK performance affect the DDS output performance?
    • Is it okay to use a frequency modulated (FM) source as my clock input to the system clock of the DDS?
    • Is there a relationship between the sample rate and the maximum update rate?
    • Learning more about Direct Digital Synthesis Technology (DDS)
    • What are the basic things to be checked when using the DDS evaluation board via external control?
    • What is the function of the SYNC_IO pin on the DDS parts?
    • What’s the function of the SYNC_CLK pin on the DDS?
    • Where can I find in the datasheet on how the output of the DDS will drift?
    • Why does a DDS need a reconstruction filter?
    • Why would I choose to use DDS for synthesizing a signal rather than a PLL?
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

Why would I choose to use DDS for synthesizing a signal rather than a PLL?

Q.

Why would I choose to use DDS for synthesizing a signal rather than a PLL?

-----------------------------------------------------------------------------------------------------------------------------

A.

Let me start with a basic comparison between the two, but keep in mind this can change over time.

In general, it is fair to say that DDS technology provides some specific advantages:  dynamic frequency and phase control is relatively easy, and is not prone to ringing or settling, so if you need to do any sweeping or hopping, DDS is a good option to start.  DDS also provides much finer tuning resolution than even a fractional N PLL can provide.  The digital nature of the DDS also makes digital synthesis more repeatable.

Conversely PLL technology offers other benefits:  Generally speaking it is less expensive and less power hungry than DDS technology.  Perhaps most importantly, you have the ability to 'upconvert' your input frequency, whereas with the DDS is a Nyquist system, and limited to providing outputs that are <50% of the sampling clock frequency that is used.

But if you look beyond the surface, you 'll find a whole lot of softening of these boundaries.  For example:  There exist both 'ping pong' and 'fast hopping' PLLs on the market (including products from ADI) which close the gap in terms of their ability to provide frequency and even phase agile outputs.  Fractional N PLLs help close the gap on timing resolution for that matter.  Conversely, ADI has also closed the gap for DDS products in some cases.  Specifically worth noting is the AD9913, which significantly closes the gap both in power and in cost to PLLs.  ADI's DDS portfolio includes many products with reference clock PLLs on board, allowing customers to upconvert their reference clock before dividing down through the DDS, meaning the output can now be a higher frequency than the reference - note is is also possible to bandpass filter a DDS output isolating a Super Nyquist image to obtain an output frequency that is higher than the reference frequency source provided.

And taking it a step further, where fractional N PLLs closed the gap in terms of frequency granularity, the Programmable Modulus mode implemented in the AD9913 (and eventually most future DDS devices), widens that gap back up.

Tags: trade_off direct_digital_synthesis direct_digital_synthesizer
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • DDS v. PLL nuances (pt I)
    DDS v. PLL nuances (pt I)
    EZ Blogs - As promised in my last post , here is [PART 1 of] a review of some subtleties of the table contrasting DDS/PLL strengths. I know I didn’t [initially] say anything about breaking this up into 2 parts, but...
  • DDS vs. PLL (round 2)
    DDS vs. PLL (round 2)
    EZ Blogs - 20 years ago I used to listen to Paul Harvey on the radio from time to time. He was known for delving deeper into news stories than many other reporters would. I enjoyed that. I hadn't thought of him for...
  • RE: How can I get an output frequency that is higher than my reference clock input frequency
    ADIApproved
    While the DDS function is inherently a frequency division, there are a couple of approaches that can be used to get a higher output frequency than the reference frequency you provide into the device. ...
 
Related Content
  • DDS v. PLL nuances (pt I)
    DDS v. PLL nuances (pt I)
    EZ Blogs - As promised in my last post , here is [PART 1 of] a review of some subtleties of the table contrasting DDS/PLL strengths. I know I didn’t [initially] say anything about breaking this up into 2 parts, but...
  • DDS vs. PLL (round 2)
    DDS vs. PLL (round 2)
    EZ Blogs - 20 years ago I used to listen to Paul Harvey on the radio from time to time. He was known for delving deeper into news stories than many other reporters would. I enjoyed that. I hadn't thought of him for...
  • RE: How can I get an output frequency that is higher than my reference clock input frequency
    ADIApproved
    While the DDS function is inherently a frequency division, there are a couple of approaches that can be used to get a higher output frequency than the reference frequency you provide into the device. ...