Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents Is there a relationship between the sample rate and the maximum update rate?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • -DDS: FAQ
    • Are any of your DDS products space qualified?
    • Are there any specific recommendations regarding via fill material in the circuit board for the thermally enhanced package styles associated with some ADI DDSs?
    • Can I use a DDS to produce modulation waveforms?
    • DDS Features Chart
    • DDS Tutorial - Introduction to DDS
    • DDS Tutorial - SINC Envelope Correction
    • DDS Tutorial - The Accumulator
    • DDS Tutorial - The Angle-to-Amplitude Converter
    • DDS Tutorial - The DAC
    • DDS Tutorial - The DAC Reconstruction Filter
    • DDS Tutorial - The DDS in Action
    • DDS Tutorial - User Guide
    • DIRECT DIGITAL SYNTHESIS (DDS) SUPPORT COMMUNITY
    • Do you recommend a linear or switching power supply?
    • Does your DDS evaluation software work on Windows XP/Vista/7/8 32-bit/64-bit?
    • How do ADI's DDS engines compare to FPGA-based DDS engines?
    • How does the REF CLK performance affect the DDS output performance?
    • Is it okay to use a frequency modulated (FM) source as my clock input to the system clock of the DDS?
    • Is there a relationship between the sample rate and the maximum update rate?
    • Learning more about Direct Digital Synthesis Technology (DDS)
    • What are the basic things to be checked when using the DDS evaluation board via external control?
    • What is the function of the SYNC_IO pin on the DDS parts?
    • What’s the function of the SYNC_CLK pin on the DDS?
    • Where can I find in the datasheet on how the output of the DDS will drift?
    • Why does a DDS need a reconstruction filter?
    • Why would I choose to use DDS for synthesizing a signal rather than a PLL?
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

Is there a relationship between the sample rate and the maximum update rate?

Q.

Is there a relationship between the sample rate and the maximum update rate?

--------------------------------------------------------------------------------------------------------------------------

A.

Yes, there is.  In a basic DDS, it is possible to update your tuning words every clock cycle.  As DDS rates have increased, though, ADI determined that interleaving multiple lower speed DDS cores to mimic a higher speed DDS core was more power efficient.  The simplest interleave would have two DDS cores and have the DDS output toggle between those two engines to effectively double the sample rate.  In order to keep the power consumption more manageable we have interleaved more and more cores to push to higher rates.

As of early 2011, the top DDS speed was 1.0 GHz (AD9858, AD9910, AD9912).  These devices feature DDS cores with 4 (AD9912) or 8 (AD9858, AD9910) slower, interleaved cores.  The DDS engine, as a whole, streams through the interleaved engines to establish the 1 GSPS rate.  To prevent glitches and avoid miscalculations in the digital domain, it is important to restrict updates of the tuning words to the point in time where the DDS engine block reverts back to the initial interleaved core, rather than allowing an update to initiate at any point in the interleave process.  This means that for a 1 GSPS DDS with an interlave factor of 8, the actual re-programming requires at least 8 ns between frequency/phase/amplitude changes

Tags: dds sample_rate