• LiDAR Solutions
    • Motor Control Hardware Platforms
    • Speech Processing Solutions
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
    Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      KCC's Quizzes AQQ301 - Counting Bicycles and Tricycles

      1. Quote of the month: " People who didn't need people needed people around to know that they were the kind of people who didn't need people" - Terry Pratchett...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 2: Achieving Phase Repeatability

    This article discusses a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents What is the function of the SYNC_IO pin on the DDS parts?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • -DDS: FAQ
    • Are any of your DDS products space qualified?
    • Are there any specific recommendations regarding via fill material in the circuit board for the thermally enhanced package styles associated with some ADI DDSs?
    • Can I use a DDS to produce modulation waveforms?
    • DDS Features Chart
    • DDS Tutorial - Introduction to DDS
    • DDS Tutorial - SINC Envelope Correction
    • DDS Tutorial - The Accumulator
    • DDS Tutorial - The Angle-to-Amplitude Converter
    • DDS Tutorial - The DAC
    • DDS Tutorial - The DAC Reconstruction Filter
    • DDS Tutorial - The DDS in Action
    • DDS Tutorial - User Guide
    • DIRECT DIGITAL SYNTHESIS (DDS) SUPPORT COMMUNITY
    • Do you recommend a linear or switching power supply?
    • Does your DDS evaluation software work on Windows XP/Vista/7/8 32-bit/64-bit?
    • How do ADI's DDS engines compare to FPGA-based DDS engines?
    • How does the REF CLK performance affect the DDS output performance?
    • Is it okay to use a frequency modulated (FM) source as my clock input to the system clock of the DDS?
    • Is there a relationship between the sample rate and the maximum update rate?
    • Learning more about Direct Digital Synthesis Technology (DDS)
    • What are the basic things to be checked when using the DDS evaluation board via external control?
    • What is the function of the SYNC_IO pin on the DDS parts?
    • What’s the function of the SYNC_CLK pin on the DDS?
    • Where can I find in the datasheet on how the output of the DDS will drift?
    • Why does a DDS need a reconstruction filter?
    • Why would I choose to use DDS for synthesizing a signal rather than a PLL?
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

What is the function of the SYNC_IO pin on the DDS parts?

Q.

What is the function of the SYNCIO pin on the DDS parts?

________________________________________________________________________________________________________________________

A.

The SYNCIO pin function is used to abort an I/O operation and reset the pointer of the serial port controller. Every completed byte written prior to a SYNCIO is preserved in the serial port buffer. After issuing SYNCIO, the SPI port expects that the next byte contains the instruction.

Example 1

Figure 1

Suppose I want to power down the DAC in AD9914. As depicted in Figure 1, Control Function Register 1 is 4 bytes wide. Without using SYNCIO, to set DAC power down would require to issue a bit stream in SPI that would look like this.

0x00 0x48 0x00 0x01 0x00

It is a one byte instruction with four bytes data. It is noticeable that a one bit change would require overwriting the whole register value. The need for flexibility in functionality arises, and that is addressed by SYNCIO. Thus issuing an instruction with SYNCIO would look like this.

0x00 0x48 (Issue SYNCIO)

 

Example 2

Figure 2

 

Suppose I have an initial value in P0 Phase/Amplitude Register(0x0C) which is:

0x45 0x80 0x0E 0x0F

Now, I want to increment the Phase Offset word by 2. This can be done in two ways; with or without SYNCIO

Without SYNCIO:  0x0C 0x47 0x80 0x0E 0x0F

With SYNCIO: 0x0C 0x47 (Issue SYNCIO)

The examples show that SYNCIO is used to eliminate the need to re-write the extra bytes in order to fill up the register value.  This means that SYNCIO can increase the efficiency in doing serial I/O operations. Lastly, the terms such as IORESET or I/O_RESET that are used by some of our DDS products are synonymous to SYNCIO. 

Tags: syncio dds