Accelerate RF Subsystem Integration with COTS SoMs and Phased Array Solutions. As building a subsystem from early prototype to full deployment is never...
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
      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Calibration Implementation Techniques for Multichannel Phased Array Subsystems

    Learn about phase-calibration techniques used for characterizing a 16 transmit and 16 receive X-band phased array subsystem based on a mixed-signal front...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents What’s the function of the SYNC_CLK pin on the DDS?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • -DDS: FAQ
    • Are any of your DDS products space qualified?
    • Are there any specific recommendations regarding via fill material in the circuit board for the thermally enhanced package styles associated with some ADI DDSs?
    • Can I use a DDS to produce modulation waveforms?
    • DDS Features Chart
    • DDS Tutorial - Introduction to DDS
    • DDS Tutorial - SINC Envelope Correction
    • DDS Tutorial - The Accumulator
    • DDS Tutorial - The Angle-to-Amplitude Converter
    • DDS Tutorial - The DAC
    • DDS Tutorial - The DAC Reconstruction Filter
    • DDS Tutorial - The DDS in Action
    • DDS Tutorial - User Guide
    • DIRECT DIGITAL SYNTHESIS (DDS) SUPPORT COMMUNITY
    • Do you recommend a linear or switching power supply?
    • Does your DDS evaluation software work on Windows XP/Vista/7/8 32-bit/64-bit?
    • How do ADI's DDS engines compare to FPGA-based DDS engines?
    • How does the REF CLK performance affect the DDS output performance?
    • Is it okay to use a frequency modulated (FM) source as my clock input to the system clock of the DDS?
    • Is there a relationship between the sample rate and the maximum update rate?
    • Learning more about Direct Digital Synthesis Technology (DDS)
    • What are the basic things to be checked when using the DDS evaluation board via external control?
    • What is the function of the SYNC_IO pin on the DDS parts?
    • What’s the function of the SYNC_CLK pin on the DDS?
    • Where can I find in the datasheet on how the output of the DDS will drift?
    • Why does a DDS need a reconstruction filter?
    • Why would I choose to use DDS for synthesizing a signal rather than a PLL?
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

What’s the function of the SYNC_CLK pin on the DDS?

A: What’s the function of the SYNC_CLK pin on the DDS?

Q: The SYNC_CLK pin is provided so the user can externally synchronize the IO_UPDATE signal and/or profile pin signals to the internal timing of the DDS core. For example, if the frequency tuning word is being continuously updated via SPI operations and consistent propagation time through the device is desired, then the IO_UPDATE must be sent synchronously to the SYNC_CLK. In addition, if multiple DDS devices are to be synchronized, a common IO_UPDATE to all parts must be synchronized to the master SYNC_CLK device.

If the IO_UPDATE signal on the IO_UPDATE pin is asynchronous to the SYNC_CLK, the pipe line delay through the device will incur an uncertainty of +/- one SYNC_CLK period.  Note, the minimum pulse width of IO_UPDATE signal must be at least one SYNC_CLK period to be registered.

If more than one profile pin is switched at a time, the profile signals are required to be synchronized to the SYNC_CLK. If not, the correct internal profile register may or may not be chosen. However, if only one profile pin is switched at a time, the profile signal can be sent asynchronous to the SYNC_CLK, but the same pipe line delay uncertainty of +/- one SYNC_CLK period will exist.

Note in most DDS products, if the profile signals are sent asynchronous to the SYNC_CLK and the wrong profile is selected, issuing an IO_UPDATE can force the correct profile setting. However, the output would have been at the wrong profile setting until the correct profile setting is forced.