Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Evaluating Power Supplies with Different Compensation Settings

    Evaluating Power Supplies with Different Compensation Settings

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents What are the basic things to be checked when using the DDS evaluation board via external control?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • -DDS: FAQ
    • Are any of your DDS products space qualified?
    • Are there any specific recommendations regarding via fill material in the circuit board for the thermally enhanced package styles associated with some ADI DDSs?
    • Can I use a DDS to produce modulation waveforms?
    • DDS Features Chart
    • DDS Tutorial - Introduction to DDS
    • DDS Tutorial - SINC Envelope Correction
    • DDS Tutorial - The Accumulator
    • DDS Tutorial - The Angle-to-Amplitude Converter
    • DDS Tutorial - The DAC
    • DDS Tutorial - The DAC Reconstruction Filter
    • DDS Tutorial - The DDS in Action
    • DDS Tutorial - User Guide
    • DIRECT DIGITAL SYNTHESIS (DDS) SUPPORT COMMUNITY
    • Do you recommend a linear or switching power supply?
    • Does your DDS evaluation software work on Windows XP/Vista/7/8 32-bit/64-bit?
    • How do ADI's DDS engines compare to FPGA-based DDS engines?
    • How does the REF CLK performance affect the DDS output performance?
    • Is it okay to use a frequency modulated (FM) source as my clock input to the system clock of the DDS?
    • Is there a relationship between the sample rate and the maximum update rate?
    • Learning more about Direct Digital Synthesis Technology (DDS)
    • What are the basic things to be checked when using the DDS evaluation board via external control?
    • What is the function of the SYNC_IO pin on the DDS parts?
    • What’s the function of the SYNC_CLK pin on the DDS?
    • Where can I find in the datasheet on how the output of the DDS will drift?
    • Why does a DDS need a reconstruction filter?
    • Why would I choose to use DDS for synthesizing a signal rather than a PLL?
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

What are the basic things to be checked when using the DDS evaluation board via external control?

Q: Most of the DDS evaluation board comes with input/output headers for ease of accessibility to some digital input/output pins of the DDS. If I want to use these pins for external control, what are the basic things to be checked?

A: Most of the DDS evaluation board has available input/output headers that correspond to some of the digital input/output pins of the DDS. To name the DDSs of which their evaluation boards has this availability are the following:

  • AD985x
  • AD995x
  • AD991x

 

Most customers access these pins but problems arise due to incorrect handling of these pins. This will serve as a guideline on what the customers will check when using the output pins and/or input pins.

Output Pins

Some DDS output pins are provided for ease of access when the user wants to monitor the output of that pin. Or, it can be used to interface with external circuitry. These pins can be used directly without having to configure the logic state of other pins. Some of these typical pins may vary on each DDS board:

  • SYNC_CLK
  • SDO
  • DROVER
  • PLL_LOCK

Input Pins

Some DDS digital input pins through the I/O headers are provided to give the customers option in controlling the DDS. The default of the evaluation board is being set-up to be controlled by the corresponding DDS evaluation software. However, a partial or complete external control to the evaluation board can be done too. Some of these typical pins are the following and may vary on each DDS board:

  • MASTER_RESET
  • EXT_POWER_DOWN
  • SCLK
  • SDI
  • CSB
  • I/O_UPDATE
  • PROFILE PINS
  • FUNCTION PINS
  • PARALLEL PORT PINS

Partial External Control

This is the set-up in which the evaluation board is first controlled using the ADI software, before shifting to external control on the DUT. The basic things to be checked are the following:

  • Set-up the evaluation board so that it is controlled by the ADI software. The user may refer to the DDS Evaluation Board User’s Guide.
  • After the DDS registers is programmed using the evaluation software, the user may now proceed to control the DUT externally.
  • Locate the Master_Reset or simply Reset pin and set to logic 0 so as not to lose the DUT register settings.
  • Make sure the EXT_POWER_DOWN pin is set to logic 0.
  • Most of the DDS evaluation boards have logic buffers between the USB interface and the DDS. There are jumpers that enable/disable these logic buffers. Locate for these jumpers and set to disable to tri-state the ICs on the evaluation board. The user may refer to the evaluation board schematic to easily identify these jumpers.
  • Selecting the profile mode can be done two ways: hardwire each profile pin to logic 1 or 0, or connect interface cable from these pins to control it externally.
  • Connect ALL the required input pins to the external circuitry via interface cable to control the DUT.
  • Set the Function Pins (applicable only to AD9914/AD9915) to the desired parallel-port configuration.

Complete External Control

This is the set-up in which the evaluation board is 100% to be controlled externally. The basic things to be checked are the following:

  • Most of the DDS evaluation boards have logic buffers between the USB interface and the DDS. There are jumpers that enable/disable these logic buffers. Locate for these jumpers and set to disable to tri-state the ICs on the evaluation board. The user may refer to the evaluation board schematic to easily identify these jumpers.
  • Connect ALL the required input pins to the external circuitry via interface cable to control the DUT. Some critical inputs are the Master_Reset and the external power down pins.
  • Selecting the profile mode can be done two ways: hardwire each profile pin to logic 1 or 0, or connect interface cable from these pins to control it externally.
  • Set the Function Pins (applicable only to AD9914/AD9915) to the desired parallel-port configuration.
  • Apply power, reference clock and control ALL digital inputs. When controlling the digital inputs, make sure that there is a defined logic state for each input. The external power down must be set to logic 0 to ensure the DDS is not in power-down mode. 
  • Send Master Reset to the DUT. This places the DDS to a known state.
  • Program the registers to the desired configuration.

May it be partial or complete external control, make sure to apply power that is within specification. The reference clock must also be referred to the datasheet for specification. Some DDS has XTAL_SEL or REF_SELECT pin that is tied low or high depending if crystal or external clock is the source of clock input. Whether the external control is using serial or parallel communication, issuing an I/O_UPDATE is always necessary when programming the registers.

  • Share
  • History
  • More
  • Cancel
 
Related Content
  • RE: AD9951 Unresponsive to SPI communication.
    ssmith
    Hi Jules.Nikko , From the listed guide, here are the things I have checked. This is the set-up in which the evaluation board is 100% to be controlled externally. The basic things to be checked are...
  • RE: Using SPI (from FPGA) to control AD9914 for single tone output
    ADIApproved
    Note, when the jumpers mentioned above are set to disable, the outputs of the ICs on the evaluation board driving the DDS are tri-stated. This to avoid BUS contention from external control. However, all...
  • AD9959 evaluation board control
    bbraverm
    Hi everyone, I have a question about the AD9959 evaluation boa rd (i.e. the AD9959/PCBZ ). In particular, is there a way to externally drive pins P0-P3 of the board in a way that has high input impedance...
 
Related Content
  • RE: AD9951 Unresponsive to SPI communication.
    ssmith
    Hi Jules.Nikko , From the listed guide, here are the things I have checked. This is the set-up in which the evaluation board is 100% to be controlled externally. The basic things to be checked are...
  • RE: Using SPI (from FPGA) to control AD9914 for single tone output
    ADIApproved
    Note, when the jumpers mentioned above are set to disable, the outputs of the ICs on the evaluation board driving the DDS are tri-stated. This to avoid BUS contention from external control. However, all...
  • AD9959 evaluation board control
    bbraverm
    Hi everyone, I have a question about the AD9959 evaluation boa rd (i.e. the AD9959/PCBZ ). In particular, is there a way to externally drive pins P0-P3 of the board in a way that has high input impedance...