Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read the Blog:  Simplified I/O: One Chip, Flexible Voltage Output, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Simplified I/O: One Chip, Flexible Voltage Outpu...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers
    Using the Industrial I/O Framework for Easy Prototyping of Software Defined Radio (SDR) Transceivers

    Introduction to Industrial I/O, libIIO, and Python software tools

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Evaluating Power Supplies with Different Compensation Settings

    Evaluating Power Supplies with Different Compensation Settings

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents Is it okay to use a frequency modulated (FM) source as my clock input to the system clock of the DDS?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • -DDS: FAQ
    • Are any of your DDS products space qualified?
    • Are there any specific recommendations regarding via fill material in the circuit board for the thermally enhanced package styles associated with some ADI DDSs?
    • Can I use a DDS to produce modulation waveforms?
    • DDS Features Chart
    • DDS Tutorial - Introduction to DDS
    • DDS Tutorial - SINC Envelope Correction
    • DDS Tutorial - The Accumulator
    • DDS Tutorial - The Angle-to-Amplitude Converter
    • DDS Tutorial - The DAC
    • DDS Tutorial - The DAC Reconstruction Filter
    • DDS Tutorial - The DDS in Action
    • DDS Tutorial - User Guide
    • DIRECT DIGITAL SYNTHESIS (DDS) SUPPORT COMMUNITY
    • Do you recommend a linear or switching power supply?
    • Does your DDS evaluation software work on Windows XP/Vista/7/8 32-bit/64-bit?
    • How do ADI's DDS engines compare to FPGA-based DDS engines?
    • How does the REF CLK performance affect the DDS output performance?
    • Is it okay to use a frequency modulated (FM) source as my clock input to the system clock of the DDS?
    • Is there a relationship between the sample rate and the maximum update rate?
    • Learning more about Direct Digital Synthesis Technology (DDS)
    • What are the basic things to be checked when using the DDS evaluation board via external control?
    • What is the function of the SYNC_IO pin on the DDS parts?
    • What’s the function of the SYNC_CLK pin on the DDS?
    • Where can I find in the datasheet on how the output of the DDS will drift?
    • Why does a DDS need a reconstruction filter?
    • Why would I choose to use DDS for synthesizing a signal rather than a PLL?
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

Is it okay to use a frequency modulated (FM) source as my clock input to the system clock of the DDS?

Q: Is it okay to use a frequency modulated (FM) source as my clock input to the system clock of the DDS

A: No.

Typically, the DDS system clock is the timing source for much of the internal workings of the DDS. A system clock with FM can introduce excessive jitter. Too much jitter will cause timing problems within the DDS device and significantly degrade performance. This is applicable to both PLL disabled and PLL enabled. Thus, the clock source must be a stable single-tone frequency source.

Tags: dds Frequency modulated
  • Share
  • History
  • More