Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain

    In this webinar, we will reassess the design of electronics for Flow Cytometry applications. In the past, 20-bit, 40 MSPS analog-to-digital converters...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Improving Industrial Functional Safety Compliance with High Performance Supervisory CircuitsPart 5: Sequencers Eliminate Systematic Failures

    This article shifts focus from managing the quantitative metrics of functional safety toward mastering the qualitative yet equally critical challenge:...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents Why does a DDS need a reconstruction filter?
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • -DDS: FAQ
    • Are any of your DDS products space qualified?
    • Are there any specific recommendations regarding via fill material in the circuit board for the thermally enhanced package styles associated with some ADI DDSs?
    • Can I use a DDS to produce modulation waveforms?
    • DDS Features Chart
    • DDS Tutorial - Introduction to DDS
    • DDS Tutorial - SINC Envelope Correction
    • DDS Tutorial - The Accumulator
    • DDS Tutorial - The Angle-to-Amplitude Converter
    • DDS Tutorial - The DAC
    • DDS Tutorial - The DAC Reconstruction Filter
    • DDS Tutorial - The DDS in Action
    • DDS Tutorial - User Guide
    • DIRECT DIGITAL SYNTHESIS (DDS) SUPPORT COMMUNITY
    • Do you recommend a linear or switching power supply?
    • Does your DDS evaluation software work on Windows XP/Vista/7/8 32-bit/64-bit?
    • How do ADI's DDS engines compare to FPGA-based DDS engines?
    • How does the REF CLK performance affect the DDS output performance?
    • Is it okay to use a frequency modulated (FM) source as my clock input to the system clock of the DDS?
    • Is there a relationship between the sample rate and the maximum update rate?
    • Learning more about Direct Digital Synthesis Technology (DDS)
    • What are the basic things to be checked when using the DDS evaluation board via external control?
    • What is the function of the SYNC_IO pin on the DDS parts?
    • What’s the function of the SYNC_CLK pin on the DDS?
    • Where can I find in the datasheet on how the output of the DDS will drift?
    • Why does a DDS need a reconstruction filter?
    • Why would I choose to use DDS for synthesizing a signal rather than a PLL?
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

Why does a DDS need a reconstruction filter?

Q: Why does a DDS need a reconstruction filter?

A: ADI’s DDSs include an integrated DAC, which converts the “numerical” sinusoid produced by the DDS to an analog sinusoid waveform like that in Figure 1.

Figure 1

This picture is an example of the DAC output signal when the DDS is generating a relatively high output frequency (approximately 1/18th of the sample DAC sample rate). This clearly illustrates the sampled nature of the DAC output. The sampled nature of the DAC output as shown in Figure 1 is the primary reason for the need of a reconstruction filter. The time domain signal in Figure 1 appears in the frequency domain like Figure 2.

Figure 2

 

In Figure 2, fc is the sampling frequency (i.e., the DDS clock frequency). The vertical black line at approximately 0.1fc represents the magnitude of the output frequency of the DDS. The vertical red lines represent the images of the fundamental, which are a consequence of sampled DDS output. Notice that there is a roll off at the frequency response of the signal before 0.5fc and the images are located beyond 0.5fc. So the role of the reconstruction filter is to significantly attenuate the images while preserving the fundamental. The result is near perfect “reconstruction” of the sinusoid signal.

This FAQ was generated from the following discussion: Why does a DDS need a reconstruction filter?

Tags: reconstruction filter dds antialias evaluation_board dac Show More