Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9830:
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • -AD9830: FAQ
    • AD9830:
    • AD9830: oscillator
    • DDS for space or Radiation Hard Specifications
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9830:

Q 

A customer wants to know if it is realy possible to have the 12bit resolution
(4096steps) with an output signal of 200kHz ?

We didn´t find this realy in the D/S.

 

A 

The ROM on the AD9830 has a 12-bit address. Therefore the 2^32 increments in
the phase accumulator are truncated into 4096 phase steps in the SINE look-up
table. In actual fact there are only 1024 values held in the sine look up
table, representing angles 0 to 90 degrees. The remaining 3 quadrants of the
sine wave are simply duplications of these values, and can be obtained by
mapping different phase inputs to the correct value  (if angle x is between 0
and 90 degrees, then input phases of x, 180-x will point to the same value, and
180+x and 360-x will point to the negative of that value).

If the phase word is 2^32/2^12 = 2^20 = 1,048,576 then the output will step
through all the values in the look up table in a single period of the sine
wave. If the phase word is greater that this then some of the values in the
look up table will be not be reached in every output wave (e.g. if the phase
word is 2 x 2^20 then every second address in the look up table will be
visited). There is a special case when the phase word is a power of 2 e.g.
2^20, 2^21, 2^22... In this case, the same addresses in the SINE lookup table
will be "visited" during each waveform and the output frequency will be an
integer fraction of the master clock frequency e.g. if the phase word is 2^21
then the output frequency will be MCLK/2048. You are not using the full
resolution of the SINE lookup table. The output can show worse spurious
spectral components in this case because the full resolution of the lookup
table (and the DAC) is not being used.

When this special case doesn't apply, then different locations in the sine
lookup table will be "visited" on every clock cycle, and over many cycles you
can expect to address every location in the SINE lookup table.

There are many variations in the "quality" of the output, depending on the
phase word employed. There are no particular rules which govern these, but
"sweet spots" exist usually where the phase word is not an even power of two.

Tags: ad9830
  • Share
  • History
  • More