Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      KCC's Quizzes AQQ297 about taking the right dose of medication

      1. First, the quote of the month: " All my life I though air is free until I bought a bag of chips " - unknown 2. New quiz AQQ297 about taking the right...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    Good Marketing Buzz, But How Do I Start?

    "AD74416H! SWIO! - Configurability! Flexibility! Wow !" Marketing is good at spotlighting key features. What it rarely answers is the practical question...

     

    Incorporating Digital Filter Modelling in LTspice Simulations

    When simulating a circuit in LTspice , the goal is likely to gain insight into the analog behaviors and trade-offs of your circuit. It is also likely that...

    Latest Blogs

    • Charting Calm Seas: Tips for Robust RS-485 Data Transmission
    • Unpacking IEC 61508: Low Complexity versus Type A Made Simple
    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9835: FSK transmitter
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • -AD9835: FAQ
    • AD9835: DC offset cancelation
    • AD9835: FSK transmitter
    • How can I perform amplitude modulation using the AD9835?
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9835: FSK transmitter

Q 

AD9835: I want to realize a frequenzy agile FSK transmitter (5 to 21 MHz,
frequency hub of +-50 or 67 kHz). It seems that the AD9835 can do this. Is that
correct an can this FSK be simulated with the evaluation board?

 

A 

In practice you can a DDS can be used to generate frequency up to approximately
one third of the input reference frequency. As you increase the output
frequency further, the filter requirements become prohibitive and
the SNR and THD start to degrade. As you are looking to generate an o/p freq of
21Mhz, this puts the AD9835 as an unsuitable choise for your application,
instead you should look at our AD9850 and AD9851.

In general, Direct Digital Synthesis (DDS) uses a crystal oscillator, Sine or
Cosine lookup table, some digital logic and a high AC performance DAC to
directly generate sine and cosine signals with of arbitrary frequency and
phase. All of the signal generation and processing is performed in the digital
domain and the high performance DAC does the conversion to the
analog domain. Because the signal is generated digitally, the phase and
frequency are very accurate (frequency resolution of 0.001Hz) and can be
changed very rapidly without the inherent lock-time required by a PLL solution.

On the AD9850, to change frequencies in your application, you need to load in a
new frequency tuning word and the DAC
starts to output the new frequency immediately after a delay of 18 clock
cycles. Programming the AD9850 is described on page 9 of the datasheet. The
AD9850 requires 5 byte writes to update the frequency register, this takes 5 x
7ns = 35ns. The latency  between updating the frequency register and the output
frequency appearing at the output is 18 reference clock cycles. In theory you
can update the output frequency in 360ns + 35ns = 395ns. In practice, you will
be
limited by the speed of your digital interface.

Whether you are using serial or parallel programming, a complete 40 bit word
must be written to the AD9850 each time the frequency register is modified.


To change the the output frequency simply use the formula

Frequency Tuning Word = ( Output Frequency x 2^32 ) / Input Clock Frequency

To calculate the new word required.

Tags: ad9835
  • Share
  • History
  • More