Open RAN 5G Radio Design: SDR SoCs for Energy-Efficient, Secure Deployments

    Building Secure and Energy‑Efficient 5G Networks with Software Defined Radios. The rapid evolution of 5G networks is driving new requirements for performance...
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
    • Power Integrity for High Performance Measurement Systems
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC Quizzes AQQ302 about Bang Gap Reference Generation

      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9851: Best value for Rset
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • -AD9851: FAQ
    • AD9851: Best value for Rset
    • AD9851: frequency senthesis
    • AD9851: RESET input
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9851: Best value for Rset

Q 

In your datasheet you show an AD9851 with both outputs connected to a
Minicircuits T1-1T transformer, the primary center-tap is grounded.

What value of Rset should be used in this configuration?

 

A 

Rset sets the full scale output current of AD9851. Output current can be set
from 5mA to 20mA with optimal performance at 10mA.

The value of Rset is related to full scale output current IOUT by Rset =
39.93/IOUT

This means approximately
2k for 20mA
4k for 10mA
8k for 5mA

A T1-1T transformer (1:1 turns ratio) can handle up to 250mW input power and
30mA DC current. The maximum output current of the AD9851 is 20mA, and with 50
Ohm termination this gives 20mW of input power. So the transformer does not
impose a limit on the output current of the DAC.

Referring to figure 9 in the AD9851 datasheet, the only case where trouble
could arise would be if the filter had a very high input impedance. The DAC has
a compliance of +1.5V maximum. If the impedance of the filter were higher than
60 Ohms OVER THE TRANSFORMER FREQUENCY RANGE 80kHz to 200MHz then the DAC
compliance range might be exceeded with a current setting of 20mA. The benefit
of the transformer coupling is that it blocks the DC component of the output
signal, so that the filter can have very high input impedance at DC without
exceeding the compliance range of the AD9851 output.

So the answer to your question depends on the impedance of the filter (compare
with figure 9) and the frequency range of the transformer. IF the filter has
moderate input impedance over the transformer bandwidth then the optimum
setting of 10mA = 3.92kOhms should be fine. Otherwise you can either reduce the
full scale output current or add a shunt resistor before the filter to reduce
the output impedance (but you lose some signal ampitude in the process)

Tags: ad9851
  • Share
  • History
  • More