Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents Ad9858: Reading data back
  • Forums
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • -AD9858: FAQ
    • AD9858: EVB VCO datasheet
    • AD9858: Output frequency change
    • Ad9858: Reading data back
    • AD9858_unused input pins connection
    • AD9858_unused power pins connection and saving power measures
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

Ad9858: Reading data back

Q 

Looking into executing readback from this device. Is the data readback from the
Buffer or Register memory? Can the device output be disabled for the entirety
of the readback, if so how? Regarding the datasheet, what exactly does the dds
core consist of?

 

A 

The data is read back from the buffer memory. All interactions by an external
processor with the device registers (read or write) are with the buffer memory.
The internal registers are updated from the buffer memory on an FUD signal.

There is no simple disable function on the device. You can setup one of the
profiles with a frequency of 0Hz and a particular phase offset, to get the
device to output a DC level when you switch to that profile. You have to select
this manually.

On page 15 of the datasheet, the DDS core is described as the part of the
device which converts the parameter settings (frequency, phase, etc) into the
samped data which is fed into the DAC. However the term DDS core can refer to
the active registers which dictate the current frequency which is being
generated, as opposed to the buffer registers which are being accessed by the
external processor.

Tags: ad9858
  • Share
  • History
  • More