Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Charting Calm Seas: Tips for Robust RS-485 Data Transmission

    by Bryson Barney As our world becomes ever more dependent on flawless digital communication, engineers need to find new ways of charting calm seas when...

     

    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

    Latest Blogs

    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9910: EVB R43 resistor value
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • -AD9910: FAQ
    • AD9910 and AD9912: Residual Phase Noise Definition and Measurement
    • AD9910 Evaluation board driver for Win7
    • AD9910 frequency update rate
    • AD9910: EVB R43 resistor value
    • AD9910: output circuit clarification
    • AD9910: output filter design
    • AD9910: Programming through SPI-Interface
    • AD9910: REFCLK termination
    • AD9910: REFCLK termination 2
    • AD9910EVB_Filter Question
    • AD9910_Multichip SYNCHRONIZATION.
    • AD9910_output amplitude flatness over frequency
    • AD9910_phase noise
    • AD9910_phase truncation bits
    • DDS_harmonic or image phase adjustment
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9910: EVB R43 resistor value

Q 

There is a question about the EVB of AD9910.
Would you kindly tell me the function of the resistor in the circle.


Is it used to do impedance match? If so, it should be 100ohm if the
transmission line is 50ohm. Is this correct?
I tested the VSWR of the AD9910's output according to our EVB.
The frequency is from 100MHz to 400MHz, but I found the VSWR is around 2 when
it output low frequency, but refer to high frequency, the VSWR is more than 3.5.
Would you kindly give some professional suggestions about how to reduce the
VSWR.

 

A 

You are correct, a 100 ohm value for R43 would be the best choice for impedance
matching.
In that case, the reflected impedance from the combination of (R7, R9, R43) at
the output of the transformer would be 50 ohms.
That would then match the 50 ohm filter with 50 load.
Note, the original intention of R43 (if used) was to remove R7 and R9 and
populate R43 only.That would eliminate resistor mismatch and possibly improve
common rejection.
If R43 is not populated, R7 and R9 would need to be 25 ohms for a proper 50 ohm
match.Some of our DDS evaluation boards are not matched. Having a higher value
termination resistor can deliver more power but the trade off is VSWR.

Attachments:
AD9910_EVBR43resistorvalue.docx
Tags: ad9910
  • Share
  • History
  • More