Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Other Products Library
    • Precision Technology Signal Chains Library
    • Software Modules and SDKs Library
    • Supervisory Circuits Library
    • Wireless Sensor Networks Library

    Latest Webinars

    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      KCC's Quizzes AQQ297 about taking the right dose of medication

      1. First, the quote of the month: " All my life I though air is free until I bought a bag of chips " - unknown 2. New quiz AQQ297 about taking the right...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Charting Calm Seas: Tips for Robust RS-485 Data Transmission

    by Bryson Barney As our world becomes ever more dependent on flawless digital communication, engineers need to find new ways of charting calm seas when...

     

    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

    Latest Blogs

    • Taming the AI Power Storm: Part 2 of 3
    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9910: output circuit clarification
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • -AD9910: FAQ
    • AD9910 and AD9912: Residual Phase Noise Definition and Measurement
    • AD9910 Evaluation board driver for Win7
    • AD9910 frequency update rate
    • AD9910: EVB R43 resistor value
    • AD9910: output circuit clarification
    • AD9910: output filter design
    • AD9910: Programming through SPI-Interface
    • AD9910: REFCLK termination
    • AD9910: REFCLK termination 2
    • AD9910EVB_Filter Question
    • AD9910_Multichip SYNCHRONIZATION.
    • AD9910_output amplitude flatness over frequency
    • AD9910_phase noise
    • AD9910_phase truncation bits
    • DDS_harmonic or image phase adjustment
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9910: output circuit clarification

Q 

About the output circuit of the AD9910 eval board , after a deeper analysis,
there are several inconsistencies and items that you may need to be aware of
and I thought you'd find this discussion interesting and useful. I've
summarized in the attached file.

 

A 

1) 75 ohm transformer in a 50 ohm circuit: Here's the word from
Andrew@minicircuits.com: When you operate a 75 Ohm transformer in a 50 Ohm
system you should expect the operational bandwidth to be slightly shifted in
frequency. So if you are using the transformer in the specified central
frequency region, there should be no practical difference. We picked this part
because of its wide bandwidth (800MHz). Because it is not operated in a 75 ohm
system, we expect this BW to decrease somewhat (according to Mini-Circuits),
but it will still be far larger than all the Mini-Circuits 50 ohm transformers
we've found.

2) If you look at the transformer's datasheet (attached here), the primary has
no center-tap (i.e., pin 5 is not used) while the secondary does. Since we need
the DDS outputs to be biased, we operate the transformer "backwards" so that
the center-tap is on the DDS side of the circuit to provide this bias. That is,
we connect the transformer such that it's secondary windings act as the primary
and vica-versa. Because this is a 1:1 transformer, this can be done without any
strange effects. We grounded pin 5 because it shorts out a potential parasitic
signal input path and was easy to do.

3) With both sides of the DDS terminated in 50 ohms, the equivalent resistance
seen at the transformer input is 100 ohms. Since this is a 1:1 transformer,
this resistance is reflected to the output of the transformer. The
reconstruction filter sees a 100 ohm source resistance. However, the design of
filter assumed a 50 ohm source and load. Because of this, the frequency
response of the filter will not be what was intended. However, if you look at
the filter's simulated response (see attached Spice simulation), it hasn't
changed much. Compared to a 50 ohm source, the 100 ohm source allows a higher
output level (because the DDS is driving a higher impedance) but also has
slightly more ripple. Note that transformer bandwidth effects have not been
included nor has the ultimate attenuation limitations of PCB stray signal paths
& non-ideal grounding.

Attachments:
AD9910_outputcircuitclarification.zip
Tags: ad9910
  • Share
  • History
  • More