Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Fast-Track Certification: Leveraging IC Safety App Notes for Functional Safety Designs
    View All Webinars
  • Community Hub

    Challenge Yourself!

      World Engineering Day Quiz!

      By Kuo-Chang A checkerboard made as a 7 x 7 matrix has a green basic cell placed in its middle as shown in the above structure. Questions: How...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9910 and AD9912: Residual Phase Noise Definition and Measurement
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • -AD9910: FAQ
    • AD9910 and AD9912: Residual Phase Noise Definition and Measurement
    • AD9910 Evaluation board driver for Win7
    • AD9910 frequency update rate
    • AD9910: EVB R43 resistor value
    • AD9910: output circuit clarification
    • AD9910: output filter design
    • AD9910: Programming through SPI-Interface
    • AD9910: REFCLK termination
    • AD9910: REFCLK termination 2
    • AD9910EVB_Filter Question
    • AD9910_Multichip SYNCHRONIZATION.
    • AD9910_output amplitude flatness over frequency
    • AD9910_phase noise
    • AD9910_phase truncation bits
    • DDS_harmonic or image phase adjustment
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9910 and AD9912: Residual Phase Noise Definition and Measurement

Q 

I used AD9852 as a LO, and found the AD9852's Phase noise is about -135dBc@
1kHz . I want to know whether ADI have products which phase noise can reach
-160dBc@1kHz? 

 

A 

The AD9912 is probably the best DDS for phase noise performance. Note, the
phase noise curves in the AD9910 data sheet are Residual measurements. That
means the REF CLK source's phase noise contribution is canceled.
An absolute phase noise measurement would include the REF CLK source's phase
noise contribution. The AD9912 data sheet has absolute phase noise curves in
all the configurations.
The reason I mentioned the residual method is to stress the measurements in the
AD9910 Data sheet assume an ideal REF CLK source.
See Application note attached AN-982: "The Residual Phase Noise Measurement"

Attachments:
AD9910andAD9912_ResidualPhaseNoiseDefinitionandMeasurement.zip
Tags: ad9910