Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    • Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card

      Important: Read the blog first . The quiz questions are all based on the content from the blog: The Power Problem Inside Every AI Breakthrough Everyone...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    The Right Switch-Mode Power Supply Control Scheme

    This article compares three switch-mode power supply control schemescurrent-mode control, voltage-mode control, and hysteretic-mode control to guide engineers...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9910 frequency update rate
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • -AD9910: FAQ
    • AD9910 and AD9912: Residual Phase Noise Definition and Measurement
    • AD9910 Evaluation board driver for Win7
    • AD9910 frequency update rate
    • AD9910: EVB R43 resistor value
    • AD9910: output circuit clarification
    • AD9910: output filter design
    • AD9910: Programming through SPI-Interface
    • AD9910: REFCLK termination
    • AD9910: REFCLK termination 2
    • AD9910EVB_Filter Question
    • AD9910_Multichip SYNCHRONIZATION.
    • AD9910_output amplitude flatness over frequency
    • AD9910_phase noise
    • AD9910_phase truncation bits
    • DDS_harmonic or image phase adjustment
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9910 frequency update rate

Q 

I am hoping to use one of your DDS devices as a chirp generator in a radar
system I am currently developing.

1) Am I correct in assuming that the AD9910 will allow me to generate a linear
frequency ramp with a frequency step time interval / update rate of 4nS ?

2) Does the AD9910 offer the fastest frequency update rate in your DDS range or
is there a faster device available ?

3) Do you have a road map which details how the frequency update rates of your
DDS devices are likely to increase in the future ?

 

A 

1) Am I correct in assuming that the AD9910 will allow me to generate a linear
frequency ramp with a frequency step time interval / update rate of 4nS ?
->Yes. The fastest frequency step time interval setting is equal to the
SYNC_CLK rate. The SYNC_CLK rate = system clock / 4. So, if the system clock is
1GHz then the period of the SYNC_CLLK is 4ns.

2) Does the AD9910 offer the fastest frequency update rate in your DDS range or
is there a faster device available ?
->If the DRG is the source of the frequency ramp, then yes the AD9910 provides
the fastest frequency step time interval setting.
However, if the frequency tuning word is provided externally on the fly for
whatever reason, the AD9915 has a full 32-bit BUS which provides a faster way
to update the 32-BIT FTW faster. In that case,
The update rate is also the SYNC_CLK rate. In that part, the SYNC_CLK is system
clock/ 16. So, if the system clock is 2.5GHz then the period of the SYNC_CLLK
is  approximately 7ns. The AD9910 cannot update the full 32-bit FTW faster than
that.

3) Do you have a road map which details how the frequency update rates of your
DDS devices are likely to increase in the future ?
->TBD

Tags: ad9910