Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9152: Phase Noise Curves and Comparison with AD9912-DDS
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • -AD9152: FAQ
    • AD9152: Phase Noise Curves and Comparison with AD9912-DDS
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9152: Phase Noise Curves and Comparison with AD9912-DDS

Q 

The customer is using AD9152 in a DDS application by generating the digital
data in a Xilinx FPGA. As indicated in AD9152 DS, Figure 31 –
The questions and answers related are specified as below.

 

A 

·          Question - As I understand the clocking is performed by SMA100A
signal generator. What frequency has the generator on the different tracks ? 
Measurements with PLL off were made with SMA100A output = 1.96608Ghz.
Measurements with PLL on were made with SMA100A output = 51MHz. 

· Question – Is the generator used at 51MHz and then multiplied to 1966.08MHz?
Yes for all the PLL on measurements

· Question – There is PLL ON and OFF curves. How are they created using
SMA100A? When the PLL is OFF, do we change the frequency of SMA100A to
1966.08MHz? Yes

· This is not a question but a comment- 51MHz SMA100A Input Signal is indicated
with legend blue but the depicted phase noise is in black. May be that requires
a correction of the legend for future DS revision. Yes this correction should
be made.

· Question-  Comparing the phase noise of AD9152 with the AD9912 DDS, Figure 23
for example gives as result that the AD9152 is 20 dB or so worse than AD9912.
Why is it so? Is it possible to reach the same level with AD9152 and a
reference with low phase noise?  The customer expect to have a 1200 MHz
reference with phase noise 1 kHz/-122, 10 kHz/-137, 100 kHz/-146, 1 MHz/-156,
10 MHz/-163 dBc/Hz. The generated single frequency shall be around 350 MHz in a
relatively narrow band  (+/- 20 MHz). What we’re seeing in the AD9152 chart is
the inherent phase noise performance limit of the DAC core. The AD9152 measured
phase noise is not coming from the clock power supply and it is not coming from
the clock source.  The AD9912 DAC core just has better phase noise performance.

Tags: ad9912