Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads

    As the Space market evolves and accelerates, mission designers need space-capable electronics that balance performance, reliability, and affordability...
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
    • Enabling New Space Missions: Commercial Space Screening Approach for Agile, High-Reliability Payloads
    • Understanding and Selecting RF Low Noise Amplifiers for Instrumentation, Phased Array and General Purpose Applications
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    Unpacking IEC 61508: Low Complexity versus Type A Made Simple

    IEC 61508 appears to include two very similar concepts. Type A and simple, which is referred to as “low complexity”. Anything that isn’t low complexity...

     

    Taming the AI Power Storm: Part 2 of 3

    Let’s peel back the curtain on how Analog Devices (ADI) is leading the charge, crafting power solutions that not only keep up with AI’s appetite but redefine...

    Latest Blogs

    • TIA Me Up, But Keep It Stable: Part 2 of 3
    • Celebrating Innovation: Top 3 EngineerZone Spotlight Blogs from 2025
    • Transforming Power: Transfer Techniques in SMPS: Part 3 of 4
    • Taming the Chaos: Correlated and Uncorrelated Sources in LTspice .NOISE Simulations: Part 3 of 3
    • ​​Where Errors Lurk in the GMSL Signal Chain​
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents Running the AD9914 faster than 3.5GHz
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • -AD9914: FAQ
    • 32-bit Resolution or 64-bit Resolution Mode
    • Achieving optimal performance from the AD9914/AD9915
    • AD9914 - connection to an uC
    • AD9914 pahse wheel and spur relationship and synchronisation query
    • AD9914/AD9915 Programmable Modulus Mode Tuning Resolution
    • AD9914/AD9915 REFCLK Multiplier
    • AD9914/AD9915 SFDR Specification
    • AD9914/AD9915 Super Nyquist Zones
    • Is the AD9914's EPAD internally connected to AGND or DGND?
    • Running the AD9914 faster than 3.5GHz
    • What is the difference between the AD9914 and AD9915?
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

Running the AD9914 faster than 3.5GHz

Q 

What will happen if I try to run the AD9914 faster than 3.5 GHz?

 

A 

The device shouldn’t just crash, but you should expect to see phase noise and
SFDR suffer as you press past the specified maximum.  Power consumption will be
higher as well.

Tags: ad9914
  • Share
  • History
  • More