Power Management Fundamentals II Session 5: Deeper Look into Power Protection

    When is the best time to discover your power circuit needs protection? Let's explore the use of some input protection and control options like ideal diodes...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Too Much Chatter and Not Enough Talk - Learn the Benefits...
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
    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

     

    ​​Functional Safety: A Driver of “Shift Left”​

    By Richard Obrien The key to faster, safer product development is to start smart - not catch up hard. In this blog, we’ll explore how the "Shift Left...

    Latest Blogs

    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
    • Automating LTspice .NOISE Measurements with .STEP and .MEAS Directives: Part 2 of 3
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents ad9951: REFCLK input considerations
  • Forums
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • -AD9951: FAQ
    • AD9951 - RefCLK using external Oscillator instead of Crystal
    • AD9951: Clock signal
    • ad9951: REFCLK input considerations
    • AD9951: REFCLK inputs
    • Eval kit for AD9951, AD9952, AD9953 and AD9954
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

ad9951: REFCLK input considerations

Q 

The AD9951 has input clock, according to data sheet it can be operated by: 1.
Crystal 2. Single ended We need to know the follow: 1. The ref clock input what
type technology it is: LVTTL/LVCMOS/LVPECL/Other 2. What voltage levels is can
accept min/max 3. Should the incoming signal need to be sine wave or square?

 

A 

This is one of those specifications that requires that we specify the part
around the way it interfaces to the outside world, not just its own
characteristics.

The input impedance is 1500 Ohms.
However, 95% of the time, customers will be transmitting the REFCLK signal down
a cable, a transmission line, a trace... Something.
When they do, we recommend that they 50-ohm terminate locally, just outside the
clock input pin, as we do on our evaluation board.

Specifying the REFCLK input voltage in dBm is an effort to convey to the
customer what oscillator strength they need back up at the front end of the
transmission line.
In short, we're looking for the user to have a maximum of 900mV pk-pk swing at
the REFCLK input.

The AD9951 reference input is normally driven with a sine wave.
It is AC  coupled (with a capacitor) and if a single-ended drive is used the
other  clock input is decoupled with another capacitor.
The drive level must  not be over 1.8 V pk-pk (0.64 V r.m.s.) with a 1.8V
supply, but may be  as low as 100 mV r.m.s.
However it is better to use as large a drive as  possible to minimise phase
noise.

If you drive the reference input with a square wave it must have a duty  cycle
of close to 50% and logic levels (for 1.8V supply) of logic 0<.4V  and logic
1>1.25V.
If you use the PLL clock multiplier with logic inputs  the duty cycle may be
slightly worse - between 35% and 65%.

Driving differentially is more recommended. Better common mode rejection is
achieved. 

However, two things to be careful about

- Common mode level of the AD9951 input :

The differential inputs are biased around 1.35V which is different from the
common mode level of LVPECL outputs.
Probably best therefore to AC-couple the clock (using series capacitors) if
using  ICS8432-101 3.3V LVPECL Frequency Synthesizer or similar.

-Jitter of the output :

You might consider using a crystal with e.g. our AD9540 clock generator, which
has <700fs clock jitter.
Otherwise, a low jitter XTAL oscillator (e.g. sinewave output) of appropriate
amplitude will provide good performance.

Tags: ad9951
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • ad9951: REFCLK input considerations
    EngineerZone
    Question The AD9951 has input clock, according to data sheet it can be operated by: 1. Crystal 2. Single ended We need to know the follow: 1. The ref clock input what type technology it is: LVTTL/LVCMOS...
  • AD9951: REFCLK inputs
    EngineerZone
    Question I would like to know what reference clock is the most adapt for the AD9951. I want to used a cristal oscillator for a high frequency stablility but I don't find in the AD9951 datasheet what...
  • AD9951: REFCLK inputs
    GenevaC
    Q I would like to know what reference clock is the most adapt for the AD9951. I want to used a cristal oscillator for a high frequency stablility but I don't find in the AD9951 datasheet what kind of...
 
Related Content
  • ad9951: REFCLK input considerations
    EngineerZone
    Question The AD9951 has input clock, according to data sheet it can be operated by: 1. Crystal 2. Single ended We need to know the follow: 1. The ref clock input what type technology it is: LVTTL/LVCMOS...
  • AD9951: REFCLK inputs
    EngineerZone
    Question I would like to know what reference clock is the most adapt for the AD9951. I want to used a cristal oscillator for a high frequency stablility but I don't find in the AD9951 datasheet what...
  • AD9951: REFCLK inputs
    GenevaC
    Q I would like to know what reference clock is the most adapt for the AD9951. I want to used a cristal oscillator for a high frequency stablility but I don't find in the AD9951 datasheet what kind of...