Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9952: Eval board
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • -AD9952: FAQ
    • AD9952: Eval board
    • AD9952: Pin connection
    • AD9952: Pin connections
    • AD9952: Pin function of 47 and 48
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9952: Eval board

Q 

Recently, I have bought Yours AD9952 evaluation board. I would, if possible,
more informations about the power supply that needs, particular the current
max, if is better
a linear than a switchin regulator. More over, using an external sine
oscillator for clock of DDS, is possible connect it directly into the balun or
need transformer for example by a PECL comparator.
Finally, what it mean DUT1 and DUT2 on the schematics, on Your data sheet there
aren't write, and so,
the PCB that You will send me at which DUT is refereed.

 

A 

The power supply requirements for the same evaluation board using the AD9954
instead of AD9952 is a stable DC supply capable of generating 1.8V, 200mA. The
AD9952 will have the same requirements.

A linear regulator not a switching regulator should be used for the power
supply. Switching type regulators should generally be avoided in powering
precision analog circuits as they require special noise control techniques.

You can connect the external sine wave oscillator for the DDS clock directly to
the balun transformer. The AD9952 reference input is normally driven with a
sine wave. It is AC coupled (with a capacitor) and if a single-ended drive is
used the other clock input is decoupled with another capacitor. The drive level
must not be over 1.8 V pk-pk (0.64 V r.m.s.) with a 1.8V supply, but may be as
low as 100 mV r.m.s. However it is better to use as large a drive as possible
to minimise phase noise. The performance of the DDS system is limited by the
quality of the oscillator. The better the performance of the oscillator, the
better the DDS performance.

DUT stands for Device Under Test, it refers to the part being tested in the
evaluation board. Many evaluation boards are common to several members of a
family of devices. If you order the evaluation board for the AD9952
(AD9952/PCB), then the DUT that you will receive in your evaluation board will
be the AD9952.

Tags: ad9952