Stop guessing, start certifying. Learn how to use IC safety application notes to streamline your FMEDA and meet IEC 61508 and ISO 13849 standards with...
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
      New KCC's Quiz AQQ298 about an interlaced square and triangle puzzle

      1. Quote of the month: " Behind every great man is a woman rolling her eyes " - Jim Carrey 2. New quiz AQQ298 about an interlaced square and triangle...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: ISO 26262 Essentials: Ensuring Confidence in Your Software...
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
    A Systematic Checklist for RF Transceiver Testing

    RF transceiver bring-up is the initial process of powering, configuring, and verifying a transceiver on new hardware to ensure basic functionality and...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Phase Sync in Digital Phased Arrays Through Direct RF SamplingPart 1: The Basics

    This article presents a methodology to synchronize multiple modular circuit boards, equipped with high speed data converters, to build a concept of a scalable...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9952: Pin connections
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • -AD9952: FAQ
    • AD9952: Eval board
    • AD9952: Pin connection
    • AD9952: Pin connections
    • AD9952: Pin function of 47 and 48
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9952: Pin connections

Q 

I have carefully looked through the data book on AD9952. Can't understand how
should I connect DACBP pin (DAC biasline decoupling pin) for AD9952. Would you
clarify this please.

 

A 

1) DACBP is normally connected to ground via a series 1uF capacitor.
You can either tie a 1uF capacitor to ground, or possibly even leave it
disconnected.
It's a bypass for the DAC reference and we haven't seen a great impact in the
performance of the device with placing a capacitor or leaving it open.

2) The AD9951 reference input is normally driven with a sine wave.
It is AC  coupled (with a capacitor) and if a single-ended drive is used the
other  clock input is decoupled with another capacitor.
The drive level must  not be over 1.8 V pk-pk (0.64 V r.m.s.) with a 1.8V
supply, but may be  as low as 100 mV r.m.s.
However it is better to use as large a drive as  possible to minimise phase
noise.
If you drive the reference input with a square wave it must have a duty  cycle
of close to 50% and logic levels (for 1.8V supply) of logic 0<.4V
and logic 1>1.25V.
If you use the PLL clock multiplier with logic inputs  the duty cycle may be
slightly worse - between 35% and 65%.

3) If CLKMODESELECT is connected to ground, the crystal out pin will be high
impedance.
     Looking at the functional block diagram on page 1 of the datasheet, the
clock out pin is driven from the output of the XTAL oscillator circuit, while
there is a separate path for an external reference clock via the MUX.


4) CLKMODESELECT can be tied directly to DVDDIO level (or through a small
pullup resistor, perhaps 1Kohm).

5) Comparator inputs .  These could be left open if you have disabled the
comparators using bit  6 of register CFR 1.
You could also terminate the inputs by putting a resistor (e.g. 50 ohms) across
them.

6) The DAC is designed to give a differential output – which results in better
performance.
If you need to convert this to a single-ended output, you should use a
diiferential to single-ended conversion circuit.
The easy way is to use a Balun (balance to unbalance transformer) ; you could
also use a suitable high speed amplifier .
(www.analog.com/highspeedamps)

Tags: ad9952