A 16T/16R X-Band Direct Sampling Phased Array Subsystem using Apollo MxFE

    Join our webinar on the Quad Apollo Platform, a cutting-edge solution for accelerating high-performance digital beamforming. Discover the ADXBAND16EBZ...
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
      1. Quote of this month: " When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content from the blog: Mature, Not Old! The Longevity of 4 – 20 mA New...
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
    ​​Where Errors Lurk in the GMSL Signal Chain​

    Whether you're debugging a stubborn camera link or designing a robust system from scratch, knowing where errors hide is half the battle. GMSL provides...

     

    Achieving Power Over Data with RS-485 Transceivers

    By Bryson Barney What if a single wire could carry both energy and information seamlessly—without either getting in the way? The future of connectivity...

    Latest Blogs

    • ​​Functional Safety: A Driver of “Shift Left”​
    • The 5 Advantages of Hardware Fault Tolerance
    • The Power Problem Inside Every AI Breakthrough: Part 1 of 3
    • Simplifying Stability with EVAL-KW4503Z: Part 1 of 3
    • Energy Transfer Considerations in Isolated SMPS: Part 2 of 4
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
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9953: How to write RAM
  • Forums
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • -AD9953: FAQ
    • AD9953: Crystal specification
    • AD9953: Design questions
    • AD9953: Generating a signal in the 50-90MHz range
    • AD9953: How to write RAM
    • Ad9953: Several issues
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9953: How to write RAM

Q 

1. What is the sequence to send to the serial port in order to write the RAM?
  
  Is it    
RamSerialAddr(0x0B) +  POW n°1 + rising_edge on IOupdate repeated for n POW
  or
           
RamSerialAddr(0x0B) +  POW n°1 + POWn°2 + ...+ POWn°n + rising_edge on IOupdate

  or
       
RamSerialAddr(0x0B) + RamAddr[0..1024] + POWn°1 + rising_edge on IOupdate ? 
repeated for n POW.

  or something else?
  
  2. I want to  first write the RAM, then I use DDS changing frequency by FTW,
and Finnally I use RAM I programmed earlier. How do I enable/disable RAM? (by
using CFR1<31> bit (Enable RAM)?). If this bit is low is it possible to write
the RAM?
  
  3. Do an easy way exists to verify that the RAM is well programmed?
(Except watch the frequency variation on the DDS output)

 

A 

1. The second option that you suggest is the correct one.
Firstly you write the control words to the RAM segment you want to address.
Then you set the PS0 and PS1 pins to select that segment.
then you send the instruction byte in the format shown on page 27 of the
datasheet, MSB is 0 for a WRITE operation, the address is 0x0B.
Then you send the sufficient number of 32bit words to fill the space defined by
the RAM segment beginning address and RAM segment end address.
The AD9953 uses the PS1~0 pins and the RAM segment control registers to work
out how many words to expect and where to place them in memory.

The 5th paragraph on the left of p 19 implies that no I/O UPDATE pulse is
required and that the RAM controller parses the values and writes them directly
into RAM.

2. If you set CFR1<31> to 0 then the RAM is powered down and will lose any
contents written to it.
To retain RAM contents, an need to set CFR1<31> to 1 and then program one of
the RAM segments in DIRECT SWITCH mode and with the start and finish addresses
identical. That way the segment will allow you to generate a sinusoid. If you
program the RAM destination bit to logic 1 then the freqency is controlled by
FTW0. See the section on direct switch mode on page 19.

3. You can read back the values from RAM by programming a 1 into the MSB of the
instruction byte.

Tags: ad9953
  • Share
  • History
  • More