Revolutionizing Flow Cytometry: 20-Bit Precision Signal Chain

    In this webinar, we will reassess the design of electronics for Flow Cytometry applications. In the past, 20-bit, 40 MSPS analog-to-digital converters...
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
    • COTS SoMs & Phased Array Solutions for Rapid RF Subsystem Integration
    • LEO Satcom: Application of RF, Mixed-Signal, & Beamforming ICs
    • 3 Real World Methods to Make Your Power Supply More Intelligent
    View All Webinars
  • Community Hub

    Challenge Yourself!

      KCC's Quiz AQQ300 about Divisibility by 6

      1. Quote of the month: " Friendship is like money - easier made than kept " - Samuel Butler 2. New quiz AQQ300 about a divisibility by 6 puzzle ...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card!

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Taming the AI Power Storm: Part 2 of 3 Test your...
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
    Clock Tree Design and Why “PLL Locked” Is Not Enough

    In high-performance RF systems, clocking architecture is a foundational element that directly governs signal integrity, synchronization, and overall system...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Multiphase Designs, Decisions, and Trade-Offs with Trans-Inductor Voltage Regulators

    This article illustrates how TLVR design choices affect performance parameters and discusses related trade-offs.

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents AD9957AD9910_Matched Latency Enable Bit
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • -AD9957: FAQ
    • 64 bit Windows compatibility
    • AD9957: maximum signal bandwidth
    • AD9957AD9910_Matched Latency Enable Bit
    • AD9957_CCI overflow
    • Can the AD9957 Evalboard and software generate CDMA modulation of the AD99957?
  • +AD9958: FAQ
  • +AD9959: FAQ
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

AD9957AD9910_Matched Latency Enable Bit

Q 

I am using AD9957, the reference clock is 48MHz, the system clock is 960MHz,
output 60MHz signal(Single Tone  Mode), and met a problem.
1. When he configured "Matched Latency Enable " Bit as 1, after power on, the
9957's output isn't stable. Sometimes there is only 60MHz signal(0dBm),
sometimes there are 60MHz,120MHz and 240MHz harmonic frequency, sometimes the
output is 240MHz(forth of 960MHz);
2. When he configured "Matched Latency Enable " Bit as 0, the output is always
correct.
Whether the "Matched Latency Enable " will influence the output? He also want
to more descriptions about "Matched Latency Enable "?

 

A 

The AD9957 and AD9910 are the same die. Bond wires separate the products
functions.
The match latency feature works on the AD9910.
A little about Match latency…...If a user wants to change two or more
parameters (frequency,phase,amplitude) at the same time and also wants that
change coincident at the DDS output, you must set the match latency bit to
logic 1. Otherwise, changes in the parameters will not be coincident.
Apparently, the AD9957 does not support the match latency feature..
The match latency bit should always be set to logic 0.

Tags: ad9957