Power Integrity for High Performance Measurement Systems

    Increasing data rates driven by AI workloads and the evolution from 5G to emerging 6G standards are placing new demands on electronic test and measurement...
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
      1.Quote of the month: "People Who Say They Sleep Like a Baby usually don't have one" - unknown 2. New quiz AQQ302 about Band Gap Reference Voltage...

    View All

    What's Brewing

      Read a Blog, Take this Quiz for Another Chance to Win a Gift Card! - Watts Going On? — The AI Power Delivery Quiz

      Important: Read the blog first . The quiz questions are all based on the content of the blog: Reimagining Power for AI: Shaping the Future of AI Acceleration...
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
    This blog presents a structured bring-up methodology for the ZCU102 + ADRV9009 platform, stepping through each initialization phase in sequence and identifying...

    New Release

    Signal Chain Designer: DC Error Simulation
    Signal Chain Designer: DC Error Simulation

    This video covers the DC error calculation capabilities of Signal Chain Designer. DC error is unique in that often requires calibration and has so many...

    Recent Technical Insights

    Latest Technical Article from Analog.com
    Game of DronesPart 1: How IMU Navigation Architectures Make or Break a Drone

    This article explains why industrial-grade UAVs require fundamentally different architectures than consumer drones. It highlights the need for inertial...

EngineerZone
EngineerZone
Direct Digital Synthesis (DDS)
  • Log In
  • User
  • Site
  • Search
OR
Ask a Question
Direct Digital Synthesis (DDS)
  • Data Converters
Direct Digital Synthesis (DDS)
Documents Ad9959: Oscillator
  • Q&A
  • FAQs/Docs
  • Members
  • Tags
  • Cancel
  • Documents
  • +AD5930: FAQ
  • +AD5932: FAQ
  • +AD5933: FAQ
  • +AD5934: FAQ
  • +AD9152: FAQ
  • +AD9830: FAQ
  • +AD9832: FAQ
  • +AD9833: FAQ
  • +AD9834: FAQ
  • +AD9835: FAQ
  • +AD9837: FAQ
  • +AD9838: FAQ
  • +AD9840: FAQ
  • +AD9840A: FAQ
  • +AD9845A: FAQ
  • +AD9850: FAQ
  • +AD9851: FAQ
  • +AD9852: FAQ
  • +AD9854: FAQ
  • +AD9854ASQ: FAQ
  • +AD9856: FAQ
  • +AD9857: FAQ
  • +AD9858: FAQ
  • +AD9859: FAQ
  • +AD9910: FAQ
  • +AD9912: FAQ
  • +AD9913: FAQ
  • +AD9914: FAQ
  • +AD9915: FAQ
  • +AD9945: FAQ
  • +AD9951: FAQ
  • +AD9952: FAQ
  • +AD9953: FAQ
  • +AD9954: FAQ
  • +AD9956: FAQ
  • +AD9957: FAQ
  • +AD9958: FAQ
  • -AD9959: FAQ
    • AD9959 evaluation board clock
    • AD9959: ADIsimDDS_spectrum
    • AD9959: FSK modulation performance
    • Ad9959: Oscillator
    • Is Data Valid Time (tDV) of 12nS for AD9959 correct? Or should it be 1.2nS instead?
    • The AD9959's SYNC_CLK has no signal. What should I check to fix this?
  • +DDS: FAQ
  • +Digital Ground (DGND): FAQ
  • +Evaluation Software: FAQ
  • +Frequency Ramp: FAQ
  • +I/O_UPDATE: FAQ
  • +Maximum Clock Rate: FAQ
  • +PLL: FAQ
  • +Programmable Modulus: FAQ
  • +SFDR: FAQ
  • +Thermally Enhanced Packages: FAQ

Ad9959: Oscillator

Q 

Is the ballon a t Pin 8 & 9 required when using an oscillator to drive the
inputs or is the ballon just used to accommodate the mismatch of the external
clock input impedance on the Eval-board?

 

A 

The Balun and the 50ohm resistor –these are for impedance matching on the input
of the AD9959.Source termination across the cable for the ext clock for eval
PCB. Also, the 50ohm source load termination does reduce the signal voltage
level by 6dB, but this is inherent in any properly terminated transmission
line. The alternative of leaving out the source termination resistor could lead
to distortion or higher jitter.

Tags: ad9959
  • Share
  • History
  • More
  • Cancel
 
Related Content
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • RE: (Video decoder)When inputting full differential, is the network resistance really 150 ohm?
    ADIApproved
    Hello Kawa, In this case, I think it is acceptable to use 75ohm as the termination resistor value for R1 on the input network for the Video Decoder. The recommendation for the 150ohm termination for...
  • RE: Differences in +/-outs in ADA4932
    HugoTUe
    Dear Charly, This is the situation: this "mismatch" or "offset" in the output signals, does not change significantly whether I use the 50ohm termination I calculated and send in the schematic, or if...
 
Related Content
  • $core_v2_language.Truncate($item.HtmlName('Web'), 200, "...")
    $author.DisplayName
    $core_v2_language.Truncate($item.HtmlDescription('Web'), 200, "...")
  • RE: (Video decoder)When inputting full differential, is the network resistance really 150 ohm?
    ADIApproved
    Hello Kawa, In this case, I think it is acceptable to use 75ohm as the termination resistor value for R1 on the input network for the Video Decoder. The recommendation for the 150ohm termination for...
  • RE: Differences in +/-outs in ADA4932
    HugoTUe
    Dear Charly, This is the situation: this "mismatch" or "offset" in the output signals, does not change significantly whether I use the 50ohm termination I calculated and send in the schematic, or if...