Post Go back to editing

AD9910 Eval Board (UG-207) — Only noise on scope, no 30 MHz output despite green status in software

Category: Hardware
Product Number: AD9910

Hello,

I'm using the AD9910/PCBZ evaluation board (UG-207) and trying to generate a 30 MHz single-tone output from a 100 MHz external reference clock, measured on an oscilloscope. I'd appreciate help troubleshooting, as I only see noise on the scope instead of a clean sine wave.

Setup:

• Signal generator (Keysight E5071C) set to output a 100 MHz CW signal, confirmed correct with 100 MHz visible on the oscilloscope directly.

• Signal generator output connected to the board's REF CLOCK INPUT (external clock, not the onboard 25 MHz crystal).

• DAC output taken from the "Unfiltered IOUT" SMA connector, connected to the oscilloscope.

• Board powered via TB1/TB2 per Table 2 in UG-207 (VCC_USB 3.3V, DVDD_IO 3.3V, DVDD 1.8V, DAC_VDD 3.3V, CLK_VDD 1.8V). Corresponding power LED is lit.

• Jumpers set for PC/USB control mode per Table 3 (W1, W2, W4 enabled; W5, W6, W3 jumpered).

• USB connected; USB status LED blinking as expected.

• Evaluation software shows all-green status, and indicates the board is connected to the AD9910.

Software configuration:

• Control window: External Clock field set to 100.00000 MHz.

• Enable Multiplier: left unchecked/disabled (bypassing the PLL multiplier, since the loop filter components are not populated on this board).

• Profiles window, Profile 0: Output Freq set to 30.000000 MHz via the Edit Output Frequency dialog.

• Enable Profile ASF: left unchecked (so amplitude runs at full scale).

• Profile 0 selected as Active.

• Clicked LOAD; the LOAD indicator shows the I/O update was sent (no longer blinking/pending).

Problem:

Despite all of the above, the oscilloscope only shows noise on the DAC output — no visible 30 MHz sine wave.


Any guidance on what else to check would be greatly appreciated.

Thank you!

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.