Post Go back to editing

AD9910 SYNC_CLK Frequency Offset Causing DDS Output Frequency Error

Category: Hardware
Product Number: AD9910

Hello Team,

I am using the AD9910 evaluation board and observing a frequency offset in the SYNC_CLK and consequently in the DDS output frequency.

My configuration is intended to provide:

  • SYSCLK = 1 GHz
  • Expected SYNC_CLK = 250.000000 MHz (SYSCLK/4)
  • Measured SYNC_CLK = 249.981124 MHz
  • SYNC_CLK error = approximately −18.876 kHz (−75.5 ppm)

249.981124 MHz × 4 = 999.924496 MHz

My questions are:

  1. What could cause this ~75 ppm offset in the AD9910 system clock?
  2. Can the AD9910 internal PLL introduce a fixed frequency offset of this magnitude even when PLL lock is indicated?
  3. Is there any recommended method to calibrate or compensate for this error?
  4. For a frequency-critical application, would you recommend using an external high-accuracy TCXO/OCXO instead of the evaluation board clock source?

The frequency measurement was taken directly at the AD9910 SYNC_CLK output.

Any suggestions on what measurements or PLL/reference-clock parameters I should check would be greatly appreciated.

Thank you.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.