Post Go back to editing

AD9914 DAC calibration time

Thread Summary

The user inquires about the DAC calibration time with a 2.4 GHz system clock, requiring a minimum of 200 μs for the DAC CAL bit to be asserted. The final answer confirms this and states that there is no upper limit for the assertion time, making a 100 ms delay due to PC interface latency acceptable.
AI Generated Content
Category: Hardware
Product Number: AD9914

Hi. I have a question about the DAC calibration time. 

We use approx 2.4GHz system clock, this means DAC calibration is time is approx 200us. This means i have to wait at least 200us between enabling and disabling the DAC Cal bit, correct ?

Does this delay have an upper limit ? Since i control the chip via a PC interface the register access is quite slow, propably 100ms between enabling and disabling the DAC cal bit. Is this a problem ?

Cheers 

Jan

Parents
  • Hi  ,

    That is correct. With a SYSCLK of approximately 2.4 GHz, the DAC calibration time is about 200 µs, so the DAC CAL bit must remain asserted for at least that duration to ensure calibration completes successfully. 

    There is no specified maximum assertion time for the DAC CAL bit. Therefore, a delay of approximately 100 ms between setting and clearing the bit, due to the PC interface latency, is not expected to cause any issues, as it is significantly longer than the required calibration time.

    All the best,

    Jules

Reply
  • Hi  ,

    That is correct. With a SYSCLK of approximately 2.4 GHz, the DAC calibration time is about 200 µs, so the DAC CAL bit must remain asserted for at least that duration to ensure calibration completes successfully. 

    There is no specified maximum assertion time for the DAC CAL bit. Therefore, a delay of approximately 100 ms between setting and clearing the bit, due to the PC interface latency, is not expected to cause any issues, as it is significantly longer than the required calibration time.

    All the best,

    Jules

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.