Post Go back to editing

AD9910 Noisy Output

Thread Summary

The user encountered a noisy and non-uniform output from a custom AD9910 board during a frequency sweep from 100 MHz to 350 MHz. The output was ~20 dB lower and had a significant dropout around 150–200 MHz. The final answer suggested checking the balun's frequency range, verifying the DAC_RSET resistor (10 kΩ to AGND), and confirming the DAC output resistors (50Ω to AVDD on both IOUT and IOUT̄).
AI Generated Content
Category: Hardware
Product Number: AD9910

I have a custom board with AD9910, with it's differential output connected to a balun and single-ended output connected to output SMA connector. I have measured it's output using spectrum analyzer while in frequency sweep mode using DRG, from 100 MHz to 350 MHz. The output is noisy and not uniform compared to the output of the ADI's Evaluation board. I have measured the output at balun's differential side, single-ended end, and at IC's pin and there is no change in the output. I have verified the register configuration by plugging in the ADI Eval. board in same setup and firmware. Can someone experience with this DDS suggest what could have gone wrong with this chip.

AD9910 Custom Board Output (Freq. Sweep, 100 MHz to 350 MHz)

AD9910 Custom Board Output (Freq. Sweep, 100 MHz to 350 MHz)

AD9910 Eval. Board Output (Freq. Sweep, 100 MHz to 350 MHz)

AD9910 Eval. Board Output (Freq. Sweep, 100 MHz to 350 MHz)

  • Hi  ,

    Apologies for getting back to you late. I have been having issues with my notification and I am trying to respond to al unanswered thread. 

    Looking at the plots, your custom board has two clear issues compared to the eval board:

    1. ~20 dB lower output power — Custom board peaks around -10 dBm vs eval board at +10 dBm
    2. Large dropout/notch around 150–200 MHz — The eval board shows a flat passband from 100–350 MHz, while your board has a deep dip

    Diagnosis:

    The notch/dropout strongly suggests a balun or matching network issue. Likely the balun's frequency response doesn't cover your full sweep range, or there's an impedance mismatch creating a resonant null at that frequency.

    The 20 dB power loss points to either:
    • Incorrect DAC output termination resistor values
    • Balun insertion loss
    • Missing or wrong value DAC full-scale current resistor (DAC_RSET)

    Recommended actions:

    1. Check your balun's rated frequency range — it may not cover 100–200 MHz properly. Compare with the eval board's balun part number.
    2. Verify DAC_RSET — should be 10 kΩ to AGND for nominal full-scale current.
    3. Verify DAC output resistors — 50Ω to AVDD on both IOUT and IOUT̄.
    4. Measure directly at DAC pins (before the balun) with a high-Z probe to confirm the issue is in the output network, not the IC itself.

    All the best,

    Jules

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.