Post Go back to editing

SDP-H1 FPGA_DONE

Thread Summary

The user encountered an issue where the FPGA_DONE LED on the SDP-H1 board did not illuminate, preventing the GUI from connecting, while using Windows 11. The problem was resolved by testing on a Windows 10 machine, indicating a Windows 11 compatibility issue. The EVAL-ADMX1001FMCZ and ADMX100X module LEDs were confirmed to be working correctly.
AI Generated Content
Category: Hardware
Product Number: admx1001

Hi. I have an SDP-H1 board connected to the EVAL-ADMX1001FMCZ board. I have installed USB drivers and all of the stuff listed in the quick start guide (https://wiki.analog.com/resources/eval/user-guides/admx/admx100x#software_needed). i powered on the SDP-Ha, then the daughter card as is specified in that wiki.    the device shows up how it should in my device manager, but the GUI cant connect to it. The FPGA_DONE LED is not illuminated, therefore i assume there is something wrong with the board or there is some sort of compatibility problem with Windows 11?    This board is fresh from the box

Parents
  • Hi daaniellee,

    Thanks for reaching out. Both the Done and Ready LED should light once the 12V supply is connected to the EVAL-ADMX100X-FMCZ.

    Can you double-check that there is no jumper connected to P10 (JTAG BOOT)? This jumper should be open during normal operation. 

    Try not connecting the SDP-H1, just the Eval-ADMX100X-FMCZ and the ADMX100X module with 12V supply. Check if both LED is turned on. 

    If you can send me picture, including the jumper settings of the board, that would be helpful. 

    Best regards,

    Emman

  • Yeah so, on the ADMX board both of the LEDs come up. its on the carrier/interface board (SDP-H1) where the FPGA_DONE led isnt illuminated.

Reply Children