Post Go back to editing

SDP-H1 FPGA_DONE

Thread Summary

The user encountered an issue where the FPGA_DONE LED on the SDP-H1 board did not illuminate, preventing the GUI from connecting, while using Windows 11. The problem was resolved by testing on a Windows 10 machine, indicating a Windows 11 compatibility issue. The EVAL-ADMX1001FMCZ and ADMX100X module LEDs were confirmed to be working correctly.
AI Generated Content
Category: Hardware
Product Number: admx1001

Hi. I have an SDP-H1 board connected to the EVAL-ADMX1001FMCZ board. I have installed USB drivers and all of the stuff listed in the quick start guide (https://wiki.analog.com/resources/eval/user-guides/admx/admx100x#software_needed). i powered on the SDP-Ha, then the daughter card as is specified in that wiki.    the device shows up how it should in my device manager, but the GUI cant connect to it. The FPGA_DONE LED is not illuminated, therefore i assume there is something wrong with the board or there is some sort of compatibility problem with Windows 11?    This board is fresh from the box