Post Go back to editing

AD9914 Spurs

Thread Summary

The user is experiencing spurs at 999 kHz and 8.012 MHz offsets from a 563 MHz output on the EVAL-AD9914 with a 3000 MHz clock. The spurs do not align with phase truncation (PT) spurs as calculated using AN-1396. The support engineer suggests trying phase dithering (not available on AD9914) and using non-rounded frequency values to potentially reduce spur levels. The user confirms that zeroing the lower 15 bits of the FTW did not eliminate the spurs, indicating they are not PT spurs. The support engineer will continue to look for documentation on these specific spurs.
AI Generated Content
Category: Hardware
Product Number: AD9914

hello,

We are using the EVAL-AD9914.

We are working with Clock = 3000MHz.

The output frequency is in the range of 500-1000MHz.

We tried to work in integer mode and in modulus mode with many different fraction (FTW, A, B) combinations.

While sweeping the output from 500 to 1000MHz we observe some frequencies that come with relatively close and high spurs.

For example:

Fclock = 3000MHz

Fout = 563MHz

Amp = full scale (4095)

We get one spur at 999kHz offset with power of -79dBc and a second spur at 8.012MHz with power of -79dBc (see attached picture).

Our requirement is to get relatively spurs free output with a span of 60MHz around the output.

We have an ability to shift the Clock Frequency and move the spurs out of this span, but we must be able to predict it mathematically.

In the above example we cannot find any mathematical equation that can help us to predict that scenario and calculate the required Fclock shift.

 Please advise :

  1. Is the above example representing the acceptable spurs level according to the datasheet?
  2. Do you have any mathematical equation that can describe the relationship between the Fclock, Fout and the spur offset from the Fout?
  3. Do you have any other method to get the DDS output without spurs in a 60MHz span?

thank you

Gil

Parents
  • Hi  ,

    I reviewed your query and replicated your setup for comparison:

    • Fs (System Clock): 3000 MHz
    • Fout (Output Frequency): 563 MHz
    • Amplitude: Full Scale

    The comparison between your setup and mine shows spur levels within an acceptable range.

    The spurs observed in the plots are not random, nor are they DAC harmonics or Nyquist images. These are phase truncation which occur due to the relationship between Fout and Fclock. Specifically how well Fout divides into Fclock.

    In terms of a mathematical equation that would describe the relationship between Fclock, Fout, and spur offset, I cannot think of any. Although I am not sure if you were able to explore our ADIsimDDS webtool. This tool tells you where the spurs are.

    At this point, I cannot identify any method to achieve a spur-free DDS output within a ±60 MHz span other than increasing the input clock frequency. However, even with the same values above, increasing Fs does not eliminate the spurs; it simply moves them to different positions. Unfortunately, I forgot to capture a spectrum image showing this movement over a wider span, but I will obtain one tomorrow and share it.

    Some thread worth reading: 

    1. AD9914 outputting more than single frequency (unknown spurs?) - Q&A - Direct Digital Synthesis (DDS) - EngineerZone

    All the best,

    Jules

  • hello Jules,

    Thank you for a detailed response.

    We are aware of the ADIsimDDS web tool.

    It shows only PPT (Primary Phase Truncation) spurs.

    I calculated the two PPT spurs for our setup (using an-1396, which discusses it).

    Fppt1=~1.972GHz and Fppt2=~1.027GHz.

    These are not the spurs we have.

    I am looking for a way to predict the 2nd and 3rd order phase truncation spurs.

    According to an-1396 they might be what we are looking for.

    And another thing:

    The 1M offset spur we see, changes power after every DAC-CAL (sometimes, go below -100dbm).

    How can that be explained?

    https://www.analog.com/en/resources/app-notes/an-1396.html

    Thanks,

    Gil

  • hello Jules,

    Adding to my above reply:

    Phase truncation occurs due to the truncation of the lower 15 bits of the phase accumulator in the AD9914.

    This results in phase truncation spurs.

    In my original message you can see the SA plot with Fo=563MHz.

    Then we zeroed the lower 15 bits. Fo slightly changed.

    However, the 8M and 1M spurs remain with same power and slightly different offset.

    See SA picture:

    Zeroing bit 16 also had no effect on the spurs.

    According to phase truncation theory, the ~8M and ~1M spurs are NOT phase truncated spurs.

    How do we proceed with finding the origin/cause of the spurs we see?

    thanks,

    Gil

  • hello Jules,

    Adding to the above:

    We identified the spurs also in Profile mode (no modulus).

    Please advise.

    thanks,

    Gil

  • Hi  ,

    Apologies for the late response. Thank you for providing me your results.  Let me compile this and I'll find a way to give you some answers. 

    All the best,

    Jules

Reply Children
  • Hi  ,

    Apologies for the late response. I will try to make this on time as possible in the upcoming queries. 

    To summarize your concerns above:

    1. Asking how to calculate higher order truncation spurs (2nd and 3rd order).

    - This was explained in the AN-1396 as you discovered. 

    2. Why a 1 MHz spur changes strength every time the DAC is calibrated?

    - This can happen because calibration adjusts internal DAC gain and matching. Small changes there can cause certain small spurs to move up or down in level each time calibration runs. 

    I believe the 552 MHz is a 1st order PPT spur (Fout-1 MHz) and the 571 MHz is a higher order PPT spur (Fout+8 MHz). 

    I have other suggestions on things might be improving these:

    1. Have you tried to turn on Phase Dither? This adds a little randomness, so the error does not repeat, and the spur disappears into a noise. 

    2. Can you try to use not rounded up number? Change the frequency by even 1 Hz? 

    All the best,

    Jules

  • Hi Jules,

    Thank you for your answers.

    My comments:

    1. AN-1396 explains how to calculate the largest first order spur, which is the PPT spur.

    It does not describe a method to calculate 2nd order PT spurs (result of the DAC harmonics) and the 3rd order PT spurs (result of the quantization spurs associated with the angle to amplitude converter and the DAC).

    2. For Fo=563MHz calculation and ADIsimDDS calculates them to be Fppt1=~1.972GHz and Fppt2=~1.027GHz.

    I wrote that I performed a test to confirm the spurs we see (~8M, ~1M) are indeed PT spurs, by loading FTW that has its lower 15 bits equal to zero. According to theory this should eliminate any PT spurs, since the 17bits the the angle to amplitude converter has not error with regard to the phase accumulator output. The spurs are still there thus we assume these are not PT spurs.

    3. I am not able to find Phase Dither in AD9914.

    Is it a hidden option in one of the control registers?

    4. I can create a frequency with FTW (profile mode) and increase the LSB by one, thus, with our 3GHz Fs, it will increase Fo by 0.7Hz.

    Do you mean input a not rounded up FTW (not a power of 2)?

    Wouldn't that introduce more spurs into the output? (since the phase accumulator will zero at different times).

    thanks,

    Gil

  • Hi  ,

    Just wanted to address your concerns:

    1. I was trying to look for some old files relating to finding how to predict 2nd and 3rd order PT spurs but I can't seem to find one. I will continue looking and will update on this thread incase I find one.

    2. I tried to zero out the right most bits as shown below to get 562.5 MHz: 

    And based on the spectrum I got, it seems like it is gone as shown:

    3. Apologies I may have overlooked the Phase Dithering part. I was referring to AD9954 not AD9914. Apologies for that and yes, you're right AD9914 does not have Phase Dither. 

    Just let me know if this works for you or we can try other things. 

    All the best,

    Jules

  • Hi Jules,

    The spurs are not always there.

    You can take the FTW for 562.5MHz, insert random ones in the lower 15 bit (that are now zero) and see if spurs appear.

    In any case, we performed the test with 563MHz (spurs were there), zeroed the lower 15 bits and spurs were still there (Fout and spurs offset slightly changed).

    According to what I understand from AN-1396, and the test we did, these are not PT spurs.

    Is there any documentation that points out to the spurs we see?

    thanks,

    Gil

  • Hi  ,

    Regarding the spurs you are seeing around the 563 MHz output in a 20 MHz span, I’m afraid we do not have any documentation that specifically identifies or characterizes these particular spurs. We also attempted to compute potential contributors based on the FTW and, similar to your findings, these do not align with PT‑related spurs described in AN‑1396.

    Based on the measurements we reviewed, the spur levels you’re seeing still fall within the published SFDR limits for the device. For this frequency range and output configuration, the datasheet typically specifies SFDR performance of < -50 dBc, depending on operating conditions. Since the spurs in your setup remain within those limits, the part is still operating within specification even though the exact equation to point out these specific spurs cannot be attributed to PT spur behavior.
    Just let me know if you have further requests.
    All the best,
    Jules