Post Go back to editing

AD9914 Spurs

Thread Summary

The user is experiencing spurs at 999 kHz and 8.012 MHz offsets from a 563 MHz output on the EVAL-AD9914 with a 3000 MHz clock. The spurs do not align with phase truncation (PT) spurs as calculated using AN-1396. The support engineer suggests trying phase dithering (not available on AD9914) and using non-rounded frequency values to potentially reduce spur levels. The user confirms that zeroing the lower 15 bits of the FTW did not eliminate the spurs, indicating they are not PT spurs. The support engineer will continue to look for documentation on these specific spurs.
AI Generated Content
Category: Hardware
Product Number: AD9914

hello,

We are using the EVAL-AD9914.

We are working with Clock = 3000MHz.

The output frequency is in the range of 500-1000MHz.

We tried to work in integer mode and in modulus mode with many different fraction (FTW, A, B) combinations.

While sweeping the output from 500 to 1000MHz we observe some frequencies that come with relatively close and high spurs.

For example:

Fclock = 3000MHz

Fout = 563MHz

Amp = full scale (4095)

We get one spur at 999kHz offset with power of -79dBc and a second spur at 8.012MHz with power of -79dBc (see attached picture).

Our requirement is to get relatively spurs free output with a span of 60MHz around the output.

We have an ability to shift the Clock Frequency and move the spurs out of this span, but we must be able to predict it mathematically.

In the above example we cannot find any mathematical equation that can help us to predict that scenario and calculate the required Fclock shift.

 Please advise :

  1. Is the above example representing the acceptable spurs level according to the datasheet?
  2. Do you have any mathematical equation that can describe the relationship between the Fclock, Fout and the spur offset from the Fout?
  3. Do you have any other method to get the DDS output without spurs in a 60MHz span?

thank you

Gil

Parents Reply Children
No Data