Post Go back to editing

How to control the amplitude of the 1G-3GHz sweep signal output in AD9915 ramp mode?

Category: Datasheet/Specs
Product Number: ad9915

Dear ADI engineer:

Hello!

Currently, I am using the AD9915 chip to output sweep signals with a frequency range of 1GHz to 3GHz in ramp mode, and have successfully obtained the expected waveform. However, in practical applications, I hope to further increase the output amplitude of the sweep signal.

In response to this requirement, I attempted the following operational approach: firstly, I utilized the OSK (Output Amplitude Control Key) function and carefully set the desired amplitude value in the profile register; Subsequently, the AD9915 was configured in ramp mode and successfully generated the required sweep signal. However, unfortunately, the above operation did not achieve the expected effect of increasing the output amplitude.

In view of this, I would like to ask if you have any other effective suggestions or methods that can help me achieve effective control of the amplitude of the sweep signal output by AD9915 in ramp mode and increase its output amplitude?

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.