Post Go back to editing

Distorted CW Output Waveform

Thread Summary

The user experienced a distorted CW signal output from an AD9959 DDS when using a 275 MHz clock and a 5th-order Chebyshev low-pass filter. The issue was resolved by reducing the DDS output amplitude to prevent driving the amplifier (PSA-8A+) into compression. The user now faces a new issue with controlling output amplitude during frequency modulation, as discussed in a previous post.
AI Generated Content
Category: Hardware
Product Number: AD9959

Hi

I'm using a AD9959 to generate a CW signal but get a very distorted signal on the output.

Details of my setup:

Clock input = 275 MHz, DDS multiplier not enabled

Output frequency = 60 MHz

Filter after DDS: 5-th order Chebyshev low-pass with cut-off at 79 MHz

I measure the following output:

Note the large amplitude variance from one cycle to the next. This looks significantly worse than what AD's simulator predicts, which is:

Any help will be appreciated.

Regards