Post Go back to editing

No output Signal

Thread Summary

The user encountered no output signal from a custom board based on the AD9953 DDS. The issue was resolved by connecting the load resistors to AVDD instead of AGND. However, the output amplitude was too high with distortion, requiring a redesign of the filter for 25 Ohm impedance. The user also noted unexpected behavior in register bits, which may have been due to writing to unused bits.
AI Generated Content
Category: Hardware
Product Number: AD9953

Hello,

I am currently trying to generate a single-tone signal with a custom board based on the AD9953.

Hardware part :

Please find my schematic below. As you can see, the loop filter is tied to GND but should be connected to AVDD. This error has been corrected with a jumper.
All supplies are ok.

PDF

Software Part:

Here is my algorithm:


1. I set  PS1, PS0, RESET, PWRDWNCTRL, IO_UPDATE, OSK_GPIO to 0
2. I toggle IO_UPDATE pin.

3. I send via SPI: 0x00 0x00 0x00 0x22 0x00, which should activate the 3 SPI pins and auto-clear the phase accumulator (register CFR1).
4. I toggle IO_UPDATE pin.
5. I send via SPI: 0x01 0x18 0x00 0x20, which should enable a reference clock multiplier of 4, register CFR2. With my 25 MHz oscillator, the system frequency should be 100 MHz. I can measure a frequency of 25 MHz on the SYNC_CLK pin.

6. I toggle IO_UPDATE pin.
7. I send the frequency tuning word: 0x04 0x02 0x8F 0x5C 0x29, which should activate the output with a frequency of 1 MHz. The frequency word has been calculated using the DDS simulator from ADI.
8. I toggle IO_UPDATE pin.

After completing all these steps, I have no output signal. I can read the AD9953 registers, and I observe something strange: bit 6 of register CFR1 is set (the "Comp power down" bit), but this is an unused bit for this device, and I am unable to disable it for an unknown reason.

Do you have any idea why I am not able to get an output signal ?

Thank you a lot for your help,

Cécile

EDIT 1 :
Below is the write signal of the software part, step 3:


The signal is coherent with the software; we have: 0x00 0x00 0x00 0x22 0x00.
Below the fourth byte.



After this, I directly read the CFR1 register to check if the value is correct. Another bit appear !
No other register has been read or written between the write and the read of the CFR1 register.

Zoom on the unwanted bit :



And finally a measurement of the io/update pin during the write sequence. I switch it two times to be sure, but there were no changes.




And finally, if I only read the CFR1 register, I have only zero's.

Edit Notes

Completed after the first reply of Jules.Nikko.
[edited by: cecile317 at 7:25 PM (GMT -4) on 16 Mar 2025]
  • Hi  ,

    Apologies for the late response.

    Is there a way you could examine the read/write SPI transactions on a logic analyzer? I just wanted to ensure that the communication between the device and the software is established and to verify if the writes are successful.

    Also, aside from this specific application, have you tried using your custom board and made it work?

    All the best,

    Jules

  • Bonjour Cécile,

    i am working with a different part. But there are similarities with the problem you reported. A first observation was with an old post from 2015 : doing 2 io updates appeared to help the values written to actually be stored. A further improvement for my case was avoiding tampering with the values of 'open' or unused bits . In the case of the ad9957 , changing some of those bits changed the values of other bits of that register. So the read back was not the same as what was written. In my case, if i understand correctly, it turned off the input rf signal. So no output was observed . I am still troubleshooting however that board.

    Henri

  • Hello,
    I have updated my original post with pictures of the SPI transaction from my oscilloscope, showing a simple write and then read of the CFR1 register.
    The communication seems to be fine. Moreover, I can set the PLL and observe the change at the clock output pin (please refer to my original post).
    However, the device behaves strangely; some bits appear and disappear, but already the same.

    Apart from the DDS, the board works perfectly. I can use the USB port, write to different memories (using a different SPI bus than the DDS), and so on.

    Thank you for your help.

    Cécile

  • Bonjour Henri,

    Thank you for your help.

    Your old post :
    SPI configuration issue
    Is really interesting...

    If I try to write 0x02 to the second byte of CFR1, I observe the following :
    - bit 6 of byte 0  in the CFR1 register is set to 1, so we have : 0x00 0x00 0x02 0x40
    - register CFR2 is set to  0x14 0x00 0x00 (MSByte first). But we should observe 0x18 0x00 0x00 instead (reset state).
    - register ASF : 0xdc 0xc0, but we should observe 0x00 0x00 at reset.
    - register ARR : 0x0e, or 0x4e, or 0x4f (the other registers are in the same configuration at each reboot/reset but this one behaves inconsistently)
    - register FTW0 : 0x00 0x00 0x00 0x00... Which is correct !

    I observe the signal with my oscilloscope, and everything is ok. I used two io/update each write/read.

    Cécile

  • Hello,

    Can you send to me the GPIO state of each pin and register configuration of the development kit in the single tone mode ?

    Thank you,

    Cécile

  • the assumption that the reset is 0 for all registers is incorrect for the ad9957 part and from what you observed, also the one you are using. .  those non reset  bits did not need any change. i changed only the bits that needed changing , after this , the part worked as expected. A read with bit level logic operations of the bits that need change appears to be all that is required

  • Hello Henri,

    I don't think that all register must be to zero too, but even these bits are different of what is given in the datasheet.

    A read with bit level logic operations of the bits that need change appears to be all that is require

    I think you are absolutely right. That's why my algorithm doesn't change any of unused bits...
    For example, the single bit set in my previous message is just to enable a GPIO needed for reading, and that's all.

    Or have I accidentally modified some unused bits?

    Kind regards,

    Cécile

  • Hello everyone,

    I finally found my mistake: the DAC is referred to AVDD, so my
    load resistors must by tied to AVDD, no AGND.

    After this modification, the DDS works as expected.

    However, my load resistor must be modified, the output amplitude is too high, with a high distortion.
    I will redesign the filter with a 25 Ohm impedance.

    Thank you everyone for your help !

    Cécile