HI
we are using AD9951 chip, in this SYNC_CLK really required for usage of single chip AD9951 if not then can i ground directly.
Regards
P Prasanth
Edit Notes
NA[edited by: Prasanth89 at 5:53 AM (GMT -5) on 24 Jan 2025]
AD9951
Recommended for New Designs
The AD9951 is a direct digital synthesizer (DDS) featuring a
14-bit DAC operating up to 400 MSPS. The AD9951 uses
advanced DDS technology, coupled with...
Datasheet
AD9951 on Analog.com
HI
we are using AD9951 chip, in this SYNC_CLK really required for usage of single chip AD9951 if not then can i ground directly.
Regards
P Prasanth
iulia - Moved from FPGA Reference Designs to Direct Digital Synthesis (DDS). Post date updated from Friday, January 24, 2025 5:52 AM UTC to Friday, January 24, 2025 1:32 PM UTC to reflect the move.
Hi Prasanth89 ,
BY default should be 0 which means SYNC_CLK pin is active. However, when activated, the SYNC_CLK pin assumes a static logic 0 state to keep noise generated by the digital circuitry at minimum. However, the synchronization circuitry remains active internally to maintain normal device timing.
To answer your question, yes, it is required to use AD9951 however, you can disable it so avoid noise generated at minimum.
All the best,
Jules
Hi Jules.Nikko
Thanking you for replying. in hardware point of view can i ground the SYNC_CLK and SYNC_IN as well disable the both in registers. then its working fine or not. please check my hardware connections attached below.
Regards
P Prasanth
Hi Prasanth89 ,
I can't seem to check your schematic as the image is too pixelated. I cannot zoom in. Can you send me a more high-definition image?
All the best,
Jules
Hi Jules.Nikko
Could you please provide PCB recommandations. PCB LAYERS, PCB Material Type.
in AD9951 Two different grounds are used so how to common both grounds. by using ferrite bead if ferrite bead used then specify the part number for ferrite bead or else any other solution is there to common both AGND and DGND
Regards
P Prasanth