Post Go back to editing

Issues in synchronising multiple AD9850 to maintain phase coherence during sweep mode.

Category: Hardware
Product Number: AD9850

Hi all,


For a current project, I need to generate at least 5 sine waveforms of the same frequency with a coherent phase relationship. This is required both during normal operation (fixed frequency) and while sweeping the frequency.

  • Sweep Requirements:
    • Frequency Range: 10kHz to at least 3MHz
    • Sweep Speed: Variable, from a few hundred microseconds to tens of milliseconds, depending on the frequency step size.
  • Implementation:
    • I'm using 5 AD9850 DDS chips.
    • Following the AD application note (AN-587), I'm using a 125MHz crystal reference clock distributed evenly and shielded to each DDS.
    • My current setup adheres to the diagrams below.
    • As recommended in the application note, I implement a common Main reset before data transfer to ensure phase coherence.
  • Observed Issue:
    • Phase coherence is only maintained for sweep times of 500ms or longer across the 10kHz to 3MHz range.
    • Slower sweeps (sub-500ms) result in a loss of phase coherence.
    • During normal operation (fixed frequency), phase coherence is maintained.
    • However, during sweeps:
  • Question:
    • Has anyone encountered similar issues with the AD9850 during frequency sweeps?
    • Are there any known techniques or workarounds to improve phase coherence during faster sweeps?
    • Is the AD9850 inherently suited for coordinated sweeps with multiple DDS chips?
  • Code Snippet:
    • Main loop:

      void loop() {

        digitalWrite(RESET_G1, LOW);
        digitalWrite(RESET_G1, HIGH);
        digitalWrite(RESET_G1, LOW);

       for (unsigned long int freq = 10000; freq <= 500000; freq += 10000) {
         setFrequencyAndPhase(freq,0);
        //Debugging: Print the updated frequency
         Serial.print("Frequency set to: ");
         Serial.println(freq);
          //Wait for 1 second before the next frequency step
          delay(500);
         }

      }

      void setFrequencyAndPhase(unsigned long int freq_in_DDS, unsigned char phase_in_DDS) {
          // Calculate the 32-bit frequency word
          unsigned long freq_DDS1 = freq_in_DDS1 * 4294967295.0 / 125000000.0;

          // Calculate the 5-bit phase word
          unsigned char phase_word_DDS1 = (phase_in_DDS1 / 360.0) * 32.0;

          // Clear signals
          digitalWrite(W_CLK_DDS1, LOW);
          digitalWrite(W_CLK_DDS2, LOW);
          digitalWrite(W_CLK_DDS3, LOW);
          digitalWrite(W_CLK_DDS4, LOW);
          digitalWrite(W_CLK_DDS5, LOW);
          digitalWrite(D7LOAD_DDS, LOW);
          digitalWrite(FQ_UD_1, LOW);

          // Send all 40 bits (LSB first)
          for (int i = 0; i < 40; i++) {
              if (i < 32) {
                  // Send frequency word (32 bits, LSB first)
                  digitalWrite(D7LOAD_DDS, bitRead(freq_DDS, i));
              } else if (i < 35) {
                  // Send control bits (3 bits, LSB first: typically all 0 for normal operation)
                  digitalWrite(D7LOAD_DDS, LOW);  // Adjust control bits here if needed
              } else {
                  // Send phase word (5 bits, LSB first)
                  digitalWrite(D7LOAD_DDS, bitRead(phase_word_DDS, i - 35));
              }
              // Clock pulse
              digitalWrite(W_CLK_DDS1, HIGH);
              digitalWrite(W_CLK_DDS2, HIGH);
              digitalWrite(W_CLK_DDS3, HIGH);
              digitalWrite(W_CLK_DDS4, HIGH);
              digitalWrite(W_CLK_DDS5, HIGH);
             
              digitalWrite(W_CLK_DDS1, LOW);
              digitalWrite(W_CLK_DDS2, LOW);
              digitalWrite(W_CLK_DDS3, LOW);
              digitalWrite(W_CLK_DDS4, LOW);
              digitalWrite(W_CLK_DDS5, LOW);
             
          }

          // Latch data with FQ_UD
          digitalWrite(FQ_UD_1, HIGH);
       
          digitalWrite(FQ_UD_1, LOW);
         
      }

I appreciate any insights or suggestions the community can offer.






The overall setup follows the AN-587, I added three more DDSs.,
I am programming them in serial mode as opposed to parallel.

Thread Notes

  • Hi  ,

    Let me address all of your questions:

    1. Has anyone encountered similar issues with the AD9850 during frequency sweeps? I did not encounter similar issues or encountered someone raised the same concerns so far. 

    2. Are there any known techniques or workarounds to improve phase coherence during faster sweeps? Aside from aligned SYNC_CLKs, IO_Update, and REF_CLK, then I believe phase coherence should not be a problem. 

    3. Is the AD9850 inherently suited for coordinated sweeps with multiple DDS chips? Yes, I believe AD9850 is suited for that. 

    All the best,

    Jules

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.