KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
AD9106
Production
The AD9106 TxDAC® and waveform generator is a high performance, quad digital-to-analog converter (DAC) integrating on-chip pattern memory for complex...
Datasheet
AD9106 on Analog.com
AD9016
Obsolete
This product is obsolete
AD9016 on Analog.com
Hi,
I am using an AD9106 to generate two sine waves. One signal is static and the other that's given a phase shift and referenced against the static signal. I am very new to the AD9106 and trying to understand what I can and cannot do. I did NOT design the board the AD9106 sits on nor part of it's selection. It is a waveform4 click board by MikroE. I know that MikroE is 3rd party and I'm not asking for troubleshooting on the hardware. But I know someone will ask for the schematic so that's what I'm using. I can only imagine that the layout is a typical or suggested layout as MikroE products are hobbyist focused.
My end goal is to give the sine waves a DC offset so that there's no negative component, i.e., if I have a 1.0 Vpp sine wave, I want to give it a +0.5 Vdc offset. I see that the chip has the DACxDOF registers which I am able to modify. However the signal I see on my o-scope doesn't line up with what I would expect. For example, if I set the DACxDOF register with a value of 0x7FF, which says it's an offset of 0.5, the the top half of the output sine wave is cut off. Reading through the datasheet, on page 26, under the DACx Digital Offset Summer, it says, "if the resulting DAC input code...exceeds full-scale, the output is clipped at IOUTFSx", and I think this is what's happening.
Okay so IOUTFSx must be clipping my signal. Let's figure out what that value is. Looking at the schematic I provided, we're using the internal voltage reference of 1.04 V (REFADJ = 0x0000). All the RSET registers are using the default value (0x0A) which is 8 kΩ. Using equations 3 & 4 in the datasheet, we have:
IREFx = 1.04 V / 8 kΩ = 0.13 mA
IOUTFSx = 32 x 0.13 mA = 4.16 mA
All this is fine, and I think I'm performing the calculating correctly, but I don't have a load on the output. It shouldn't be exceeding IOUTFSx and thus shouldn't be clipping.
If none of this is possible with the AD9106, I am able to use an external circuit to give the signal the DC offset I'm looking for. However, software would be easier.
Side note, what does a digital offset of 0.5 mean? There's no units with it. I assume it means a positive shift of half the output. 0x400 would be a positive shift of a quarter of the output. That's another question.
Thank you.
Hi mattdrsbh ,
Apologies for the delayed response. We're currently looking into this and we'll get back to you in a few days. Just a quick question, do you also have the AD9106 Evaluation Board with you?
Best regards,
Marco
Hi mattdrsbh,







Hi Alex,
Thank you for taking the time to read my post and provide an answer. I do appreciate it. I unfortunately had to pivot in the design due to technical issues beyond the questions I asked. I have saved this information so I can reference it next time.
Also I don't have the eval board, but I will get one. You are not the first person to ask me that.I get the impression being able to play around with one will allow me an easier path to troubleshoot any issues I run into.
Thanks again.